cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSO SPI communication problem

gabriel.arnautu
Associate II

Good morning,

I am trying to read the WHO_AM_I register from LSM6DSO, but it doesn't respond as needed. I will attach a picture from signal analyzer (D0 is CS, D1 is CLK, D2 is MISO, D3 is MOSI). It looks like its respond is 0x50 instead of 0x6C. What should I change?

I tried with a MAX32630 and it was working (8 bits transfer mode).

When I try with RS14100 (16 bits mode) it responds with 0x50 instead of 6C.

Gabriel

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
S.Ma
Principal

If it is still the same as before, MEMS start in SPI 3 wires. First write the control register to go to 4 wires, then read back the WHO_I_AM, or manage the SPI 3 wire by shorting MISO and MOSI on the same line.