MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DH Low-power mode

LIS3DH MEMS digital output motion sensor.Hi every body.I'm using this sensor in 'High-resolution mode'. but after some time (I define timeout = 10 seconds) without detect any motion, put the sensor in 'low-power mode'. if the sensor is moved before t...

LM by Associate II
  • 1209 Views
  • 1 replies
  • 0 kudos

Chipselect used as I2C reset

Many ST mems sensors allow the user to select an I2C or SPI serial interface by controlling the chipsel (CS) pin.My question is: in case a sensor, used as an I2C slave, gets stuck waiting for the master to acknowledge the read operation, does togglin...

GioP by Associate II
  • 1986 Views
  • 3 replies
  • 0 kudos

Which pin does slave address of LSM9DS-magnetometer depend on ?

I was going through datasheet of LSM9DS1 (DocID025715 Rev 3) at page# 30/72 according to table-20, the bit number 1 of slave address (SAD) depends on SA1 but I couldn't find what SA1 is any where in the document. While in page# 11/72 according to tab...

AJk by Associate
  • 1880 Views
  • 3 replies
  • 0 kudos

How to create Device.mk file for LSM6DSL for Android Sensor HAL

According to STMicroelectronics guide on github STMems_Android_Sensor_HAL_Input I'm unable to find device.mk file from <AOSP_DIR>/device/<vendor>/<board>/device.mk.Should i need to make this file at this location ?If yes then what are required to wri...

MAmba by Associate
  • 835 Views
  • 0 replies
  • 0 kudos

Resolved! Wake-up for low power application

We are working on a very low power device which requires a "wake up" interrupt utilizing a "cost effective" device. I have initially started looking at the LIS3DE which has two interrupt outputs.We essentially are in an active (VCC is on), with low p...