MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SensorTile.box #1: Connect your box and start - HW overview

We'll start with connecting your smartphone via Bluetooth with the SensorTile.box. The tool is provided with Bluetooth® Low Energy v4.2 application processor module (SPBTLE-1S) that enables the BLE communication. Connect the tool with your charger (e...

Raspberry Pi, SPI issues Lsm6dso

Does anyone have any experience getting the LSM6DSO to talk to a raspberry pi via SPI. Ive setup my system with the BCM2835 library which allows to me to make a read and write function. Using an oscilloscope Ive monitored the data returning from the ...

MBond by Associate II
  • 1213 Views
  • 1 replies
  • 0 kudos

LIS3DH - Current drive by SO pin

Hi,My LIS3DH share SPi bus with an other component which has an internal pull-up (arround 15kOhm).When I start a communication with my LIS3DH, SO pin never be at 0V. I see drop voltage arround 0.5V, on SO pin. SI and CLK pin's level are ok.I have dis...

G.Lumeau by Associate
  • 859 Views
  • 1 replies
  • 0 kudos

stm32f7 + VL53L0

I can’t figure out how to work with this sensor. All documentation on it is extremely complex and incomprehensible (I have a VL53L0 sensor and a stm32f745 microcontroller. Could anyone be amazed at the quick start example, I don’t know where to start...

LSM9DS1 G threshold is 8 bit but X, Y & Z are 16 bit values

Trying to determine how I set an acceleration threshold when the threshold register is half the size of the acceleration vector registers.The gyro makes sense as the threshold for it is the same size as the 3 vector registers but the G sensor just do...

Where I can find iNEMOEngine_LI3?

Hi, I'm developing an application with stm32F401 nucleo board and the expansion board iks01a3. I'm using the motion_fx library and it works very well but I would like to download the library iNEMOEngine_LI3 (lite version) to see how kalman filter wor...

Symon by Associate II
  • 1399 Views
  • 1 replies
  • 0 kudos

Matlab sensor fusion toolbox - IMU parameters

Hello,We are looking to use the extended Kalman filter within the Matlab sensor fusion toolbox.There are some accel/gyro noise parameters required by the imufilter() function within that collection of functions. They don't appear to be commonly inclu...

MKear by Associate II
  • 1311 Views
  • 1 replies
  • 0 kudos