MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problems with temperature affecting the readings from LSM6DS3TR.

I'm developing a product using the LSM6DS3TR. As per the data sheet the data from the device should not be influenced by temperature more than 1.5% between -40 and +85 degrees. I see wild swings in the data for the Y-Axis Accelerometer when the tempe...

RConw by Associate II
  • 3501 Views
  • 5 replies
  • 1 kudos

LIS3DH using too much power on custom board

I have a custom board that includes the LIS3DH. With the LIS3DH not populated, my board uses 0.009mA, but with the LIS3DH populated and not configured, it uses 0.135mA. According the data sheet, it should be 0.011mA. The data sheet also says the LIS3...

0690X00000BuYGJQA3.png
SKein.1 by Associate
  • 886 Views
  • 1 replies
  • 0 kudos

hts221

When the hts221 passes the test, the humidity of the constant temperature and humidity box is adjusted to above 70% (the temperature of the constant temperature and humidity box is not set to a specific degree), which is very inaccurate.In particular...

IIS2DLPC wake up interrupt bit always set?

it seems that the status bits in the registers for wake up are always active - Is it possible to remove them? If I setup the part to wake up routing the wake up to INT1, then issue a soft reset to the device, setting it up next to just route the DRDY...

DMede.1 by Associate
  • 1154 Views
  • 1 replies
  • 0 kudos

VL53L1X - Using SPAD for 3D Topology

Hello St Community,We would like to use the VL53L1X to get a series of measurements in a 4X4 SPAD array to graph the 3D Topology of an object. We have already set the ROI and FOV. I was wondering how we could do this? Are there any relevant code exam...

HKara.4 by Associate II
  • 1593 Views
  • 5 replies
  • 1 kudos

How to setup FIFO for LIS2HH12?

I am using LIS2HH12 with Atmel ATSAM4E8C and am able to read registers and write to registers.When I read FIFO_SRC register (0x2F) I get Bit EMPTY=1 and in STATUS register (0x27) ZYXDA is constantly 0. I am following the example from https://github.c...