MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I want to decrease the power consumption of LIS2DW12. It proposed to sense human motion, and I don´t know if it is better to have a Low Pass Filter or High Pass Filter configured in CTRL6, and what LPM mode I should set in CTRL1. Please see details below:

Actually our device has 33 uA in DC current consumption without accelerometer LIS2DW12, with the LIS2DW12 this previous number increases to 55 uA.I think that it is possible to decrease the current consumption, based of the information of datasheets....

JGonz.1 by Associate II
  • 1764 Views
  • 3 replies
  • 0 kudos

Do all current consumption of lis2mdl tested in 2.5V?

In the spec, Table 10 and Table 11 show's the current consumption when LIS2MDL working in different modes. But it doesn't verify the test voltage. Please help to confirm if they were measured in 2.5V. Thank you!

Czhan.15 by Associate
  • 1216 Views
  • 1 replies
  • 0 kudos

Problems with temperature affecting the readings from LSM6DS3TR.

I'm developing a product using the LSM6DS3TR. As per the data sheet the data from the device should not be influenced by temperature more than 1.5% between -40 and +85 degrees. I see wild swings in the data for the Y-Axis Accelerometer when the tempe...

RConw by Associate II
  • 3392 Views
  • 5 replies
  • 1 kudos

LIS3DH using too much power on custom board

I have a custom board that includes the LIS3DH. With the LIS3DH not populated, my board uses 0.009mA, but with the LIS3DH populated and not configured, it uses 0.135mA. According the data sheet, it should be 0.011mA. The data sheet also says the LIS3...

0690X00000BuYGJQA3.png
SKein.1 by Associate
  • 857 Views
  • 1 replies
  • 0 kudos

hts221

When the hts221 passes the test, the humidity of the constant temperature and humidity box is adjusted to above 70% (the temperature of the constant temperature and humidity box is not set to a specific degree), which is very inaccurate.In particular...

IIS2DLPC wake up interrupt bit always set?

it seems that the status bits in the registers for wake up are always active - Is it possible to remove them? If I setup the part to wake up routing the wake up to INT1, then issue a soft reset to the device, setting it up next to just route the DRDY...

DMede.1 by Associate
  • 1131 Views
  • 1 replies
  • 0 kudos