MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

why my lis3dh current consume is bigger than spec?

​1 :i only use the Lis3dh ,and remove all other elements ​2: i use the power 3.0V, i use multimeter test the current consume between VCC and GNDget the test result current is 16 μA,(the spec says ,the device automatically enters power-down mode, a...

0690X00000AQwXKQA1.png
xxuej by Associate
  • 1106 Views
  • 2 replies
  • 1 kudos

Resolved! How do i get L3GD20 Gyro sensor to work on STM32L0?

Hello, I am simply tring to communicate with the L3GD20 Gyrosensor using the WhoAmI command. I am sending 0x0F and i'm expecting 0xD7 back (11010111) but I only received 0xFF which means i'm doing something wrongI am using STM32CubeMX to generate the...

MikeP by Senior
  • 1533 Views
  • 1 replies
  • 0 kudos

I have problem with IKS01A2_LPS22HB_FIFOMode application generated by CubeMX. There are things in the code that i have to change.

I've generated project for SW4STM32 and i don't know that to do with iks01a2_conf_template.h file. Im supposed to replace the header file names with the ones of the target platform and rename the file to iks01a2_conf. There are 3 headers:#include "s...

CD.1 by Associate
  • 1053 Views
  • 1 replies
  • 0 kudos

Source code for ST.COM's X-CUBE-MEMS1 available?

Is the source code for ST.COM's X-CUBE-MEMS1available? I am using an STM32L412. And when I try to include the STM32 pre-compiled library into my project I get errors. I am thinking the processor I am using is not compatible with the libraries. So I...

Rstua.1 by Senior
  • 3730 Views
  • 9 replies
  • 0 kudos

How to connect more LSM303AH on one SPI BUS?

We are affraid when one device has CS signal down, other devices will be set to I2C there can be conflict on the SPI BUS. Is it possible connect more devices as eclosed schematic?

Using X-CUBE-MEMS1 for lsm9ds1

Hi, I want to use -CUBE-MEMS1 for lsm9ds1. By default the applications code uses LSM303AGR . Could any one give me some hints what changes I need to do for porting ECompas application for lsm9ds1. I have already ported the driver accelerometer, gyro...

Resolved! LIS2DH false positives in detection of clicks

Hello all,I am having an issue with single-click detection. I am getting false click detections at certain threshold values. I found this out yesterday when I had an MCU register lots of clicks repeatedly, but the device was not being shaken.To test,...

(LSM6DSL) how to get total G-Force

(Because I am not good at English, I used Google Translator.)​I'm using the LSM6DSL sensor now. I think that with this sensor still, the total gravity acceleration should be 1G, or 9.8.( Total - G - Force = SQRT(x^2 + y^2 + z^2 ) ) ​However, as the s...

Edoyo.1 by Associate
  • 1263 Views
  • 1 replies
  • 0 kudos