cancel
Showing results for 
Search instead for 
Did you mean: 

Is the STMicro's LSM9DS1 chip supported by STMicro "Middleware" software?

Rstua.1
Senior

I am interested in utilizing vetted STMicro LSM9DS1 software calibration tools and other STMicro "Middleware".  I had assumed STMicro would support their own chip in order to encourage sales. But, the STMicro's LSM9DS1 chip is not supported in X-CUBE-MEMS1 according to the release notes found here (LSM9DS1 is not to be found anywhere in this document):

file:///C:/Users/ricks/proj/st/x_cube_mems1/en.x-cube-mems1/STM32CubeExpansion_MEMS1_V7.0.0/Release_Notes.html

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
KnarfB
Super User
Rstua.1
Senior

Thank you @KnarfB​ for your response. I looked through the sub directory "lsm9ds1_STdC" of the STMems_Standard_C_drivers you pointed to which contains the driver code for the STMicro LSM9DS1 chip. I see code to access the LSM9DS1. but I don't see any "Middle Ware" code. Such as code to implement electronic compass tilt compensation. Code which I believe exists in STmicro's X-CUBE-MEMS1 package. But X-CUBE-MEMS1 does not appear to support STMicro's own LSM9DS1 chip. Specifically, I'm looking for LSM9DS1 chip support similar to what is found in the STM32_MotionEC_Library found here: en.x-cube-mems1\STM32CubeExpansion_MEMS1_V7.0.0\Middlewares\ST\STM32_MotionEC_Library when expanding the X-CUBE-MEMS1 zip file from STMicro.

Miroslav BATEK
ST Employee

The Middleware libraries are sensor agnostic so basically you can use them with any sensor.

The LSM9DS1 is not supported in X-CUBE-MEMS1 package but you can write your own firmware using the LSM9DS1 driver and the MotionEC library.

Rstua.1
Senior

This is good news. I am already communicating with the LSM9DS1 using the drivers STMicro maintains on Github.com. Above that, I wrote code to derive the compass heading. But only for the simple case where I am using the X & Y magnetometer (where Z is always pointed down toward the earth). So, you are saying I can give that data to X-CUBE-MEMS1 (the MC for compass calibration & EC for compass heading) and in return get back the heading from a calibrated compass! That would be great!

Assuming these are the two correct drivers to use for calibrating a compass and calculating the compass heading - are there any examples where they are used? I was looking through the examples packaged with X-CUBE-MEMS1 and did not come across a compass heading example.

-thanks

Miroslav BATEK
ST Employee

Correct, you should use MotionMC (Magnetometer calibration library) and MotionEC (eCompass) for device orientation. The heading can be then calculated from the outputs from MotionEC library. Please check ECompass application in X-CUBE-MEMS1 package, you can use it as example or reference for you project.