MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL MKI109V3 Unable to enter DFU

Hello I have installed Unico and DFUSE DEMO and all the drivers, and when I connect my board to the PC I can see the virtual com port 6:but when I open dfusedemo, and press button 3 and 2 together then release 3 then 2, I get this:I can't get the S...

0690X00000DYV4nQAH.png 0690X00000DYV57QAH.png
WGeng.1 by Associate II
  • 1497 Views
  • 2 replies
  • 0 kudos

www.st.com

Dear community,I found the Q&A but I can't find the place where I can write my own question. So I do it here for now.I have a question about the vl53l0x api. In the API manual they say that you should call it in this sequence:dataInit()staticInit()Pe...

Rvalk.1 by Associate
  • 705 Views
  • 0 replies
  • 0 kudos

MEMS asm330 lhh Power-on PIN INT1 setting

Hi!I'm reading the official asm330lhh datasheet. There is a sentence "INT1 must be set to '0' or left unconnected during power-on" under Table 17 in Chapter 7. This sentence means that when MEMS is powered on, ensure that INT1 is at 0 level or Does t...

0690X00000DXQ5eQAH.jpg
CLiu.2 by Associate
  • 1628 Views
  • 2 replies
  • 0 kudos

Resolved! Sensortile.box Unable to build FP-SNS-ALLMEMS1

Hello all,I recently got the sensortile.box and was trying to play with the all mems function pack (FP-SNS-ALLMEMS1) but had trouble building the project. I have added an image of the error that I get when I try to build the project. I was able to fl...

0690X00000DXDR3QAP.png
VRao.1 by Associate III
  • 2560 Views
  • 3 replies
  • 0 kudos

Unico v9.3.0.0 missing 'ProfiMEMSToolV3.6.13.bin' file?

I downloaded the latest Unico (en.stsw-mki109w.zip) and unpacked it. Since I'm running Windows, I followed the instructions to install STM32CubeProgrammer. But when I try update the firmware, there is no .bin file in the archive. It only contains a ....

0690X00000DYOFoQAP.png
SBrow by Associate
  • 1369 Views
  • 2 replies
  • 0 kudos

Resolved! Multiple event detection on LSM6DSOX

I am developing a driver for LSM6DSOX. According to the datasheet, the module is capable of detecting free-fall, wakeup, motion detection, activity/inactivity, and so on.Is it possible, to configure multiple event detection interrupts (especially sin...