MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use STEVAL-STLKT01V1 SensorTile with ANN?

Hi,I get a  STEVAL-STLKT01V1 development kit and I try to run ANN on the board. I have some questions about using it.To program the board, an STM32 Nucleo board is essential? If not. Now, I have embeded the pro-trained ANN in the MCU by connecting a...

Kchen.1 by Associate
  • 1185 Views
  • 2 replies
  • 0 kudos

Resolved! How to read E-compass on STM32F3DISCOVERY board?

Hi, I'm evaluating on the STM32F3DISCOVERY board using STM32CubeIDE but I'm having trouble interfacing with the onboard E-compass. In the Device Configuration Tool, I've enabled I2C1, since the user manual states that the MCU controls the E-compass v...

RLee.2 by Associate II
  • 2767 Views
  • 3 replies
  • 0 kudos

Cannot get data from the SensorTile.Box into the Watson IoT Platform

I am using Algobuilder to setup a dumb application to get the acceleration from the SensorTile.Box. I compile it using the BLE template and connect the box ST BLE Sensor Android App. The connection between the App and the Watson IoT Platform is corre...

GRobl by Associate II
  • 1016 Views
  • 2 replies
  • 0 kudos

Problem with sensor and freertos

Hi i have a problem. When i use a sensor with freertos and i put in the same task the function to read the value from the sensor and the osdelay() my task do one misuration and after do nothing. I print the value with the HAL_UART_Transmit.

TILEBOX - Proper charging behavior??

The User Manual states the RED flashing LED indicates the battery is charging but I'm not so sure about this. First, it appeared that I could not get any charging at all unless the the ON button was depressed for a few seconds. It also appears that...

0693W0000000B4lQAE.jpg 0693W0000000B4qQAE.jpg 0693W0000000B5KQAU.jpg
TJM by Senior II
  • 1418 Views
  • 3 replies
  • 0 kudos

Deformation measurment of metall reactor

Dear all, ​I am interested in the MEMS accelerometer (IIS3DWB) to measure radial and maybe vertical movement of a metall reactor. The maximum g range of the movement should be 4-5 g. And the vibration frequency should be 0.5-2 kHz. I would install a...

Fur.1 by Associate II
  • 2139 Views
  • 4 replies
  • 0 kudos

The STM32CubeExpansion_MEMSMIC1_V5.2.0 demonstration firmware converts PDM mic data to PCM and sends it on the USB OTG port. I was wondering if I could get access to the .ioc CubeMX file for the same.

I am using the STM32L476RG nucleo board with the CCA02M2 EVM. For ease of experimenting with the clock and audio parameters, I wanted to have access to the cubeMX .ioc file that would show up in the file explorer of cubeIDE.I have attached the files ...

KAbis.1 by Associate II
  • 1284 Views
  • 1 replies
  • 0 kudos

Removing unused sensors from the STEVAL-BCN002V1B board

I'm working on a low powered bluetooth prototype that has several power constraints. I'm thinking of using the STEVAL-BCN002V1B design as a reference point and I excluded several unused sensors by my project requirements. Will the default firmware st...

HChun.1 by Associate
  • 1051 Views
  • 1 replies
  • 0 kudos