cancel
Showing results for 
Search instead for 
Did you mean: 

How to remove Gravity factor from Accelerometer readings .

PD_learner
Associate II

 I am using the industrial IIS2DH accelerometer in my vibration analysis product. I need only pure acceleration values in all directions. So at any state if the device is stable (or in constant speed), it should give (0.0,0.0,0.0) roughly.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Ozone
Principal III

Measure at rest, store as calibration value, and subtract at runtime.

Eleon BORLINI
ST Employee

plz check also this thread, if can be of your interest. You could apply the embedded IIS2DH HP filter (CTRL_REG2 (21h) bits, see p.34 of the datasheet), if you need to monitor only acceleration variation above a certain frequency. But as per similar threads, Ozone suggestion must be the preferred one. Regards