MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

H3LIS100DL sleep-to-wake - how to enable?

Greetings. I am familiar with the general sleep-to-wake functionality, I've used it successfully in the IIS2DH. However I am having issues with the H3LIS100DL. I believe I've enabled sleep-to-wake using control register 5, I've configured the interru...

cphelan by Associate II
  • 1644 Views
  • 2 replies
  • 0 kudos

How does Generic MQTT Cloud Logging work

Hi! I am using a SensorTile.box and tried to enable Generic MQTT Cloud Logging. Unfortunately I could not get any data to one of the public brokers. I used for example "tcp://mqtt.eclipse.org" Port 1883 (the tcp:// is mandatory, otherwise it won't wo...

DWind.1 by Associate III
  • 1560 Views
  • 2 replies
  • 0 kudos

ISM330DLC (LSM6DSM): Current consumption & wake-up time ?

About: ISM330DLC (LSM6DSM)What is current consumption of Gyro sensor in sleep mode?What is wake up time from sleep mode? (sleep mode mentioned in AN5125 para 3.5 & DS12171 rev 3 Table 3 section 4.2) Thanks for your help

CHarr.1 by Associate II
  • 1170 Views
  • 1 replies
  • 0 kudos

How to reset the STEVAL-MKSBOX1V1 kit

Morning everybody, I have a STEVAL-MKSBOX1V1 kit, after flashing the microcontroller with an example of ST applicati I can't connect in bluetooth with my smartphone.Could you tell me how to reset the STEVAL-MKSBOX1V1 program to factory default. I tri...

SAbid.2 by Associate II
  • 2084 Views
  • 4 replies
  • 0 kudos

How to read temperature data from lis3dh?

Refer to lis3dh datasheet, I setting bit 7 and bit6 to 1 in TEMP_CFG_REG, but the data I read from OUT_ADC3_L always 0x40/0x80, OUT_ADC3_H always 0xff. Anything wrong in my config?Thanks.

LPeng.1 by Associate
  • 1685 Views
  • 3 replies
  • 0 kudos

What is the frequency range of LSM6DSL sensor?

Hi, I am using LSM6DSL Click Board to measure an expected frequency of 1hz. The datasheet seems to be very vague on this, or I might have missed it. If anyone knows on this information, please share. Thanks

SNik.1 by Associate II
  • 2401 Views
  • 4 replies
  • 0 kudos

Resolved! 404 when accessing AN4987 application note

I am having a hard time configuring the LIS2MDL via the sensorhub on the LSM6DSM. The datasheet gives very little information. I would like to check the application note but I can't reach it.

MScho.3 by Associate
  • 1924 Views
  • 1 replies
  • 0 kudos