Hi, I am using LSM6DSL Click Board to measure an expected frequency of 1hz. The datasheet seems to be very vague on this, or I might have missed it. If anyone knows on this information, please share. Thanks
Hi @Eleon BORLINI ,I am using only Accelerometer and have powered down Gyroscope. The settings are: ODR = 6.66KHZ, Full Scale = +-2g, Analog bandwidth filter (BW0_XL = 0) = 1.5kHz, Bandwidth = ODR/2 (As shown in the picture below)I have set TIM2 ...
Hi @Eleon BORLINI Thank you for the clarification. The LSM6DSL Click Board is set up to communicate to STM32F767ZI-NUCLEO through I2C. I guess the root to my question is to find out whether LSM6DSL is sensitive enough to detect 1Hz vibration freque...