MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use STEVAL-STLKT01V1 SensorTile with ANN?

Hi,I get a  STEVAL-STLKT01V1 development kit and I try to run ANN on the board. I have some questions about using it.To program the board, an STM32 Nucleo board is essential? If not. Now, I have embeded the pro-trained ANN in the MCU by connecting a...

Kchen.1 by Associate
  • 1154 Views
  • 2 replies
  • 0 kudos

Resolved! How to read E-compass on STM32F3DISCOVERY board?

Hi, I'm evaluating on the STM32F3DISCOVERY board using STM32CubeIDE but I'm having trouble interfacing with the onboard E-compass. In the Device Configuration Tool, I've enabled I2C1, since the user manual states that the MCU controls the E-compass v...

RLee.2 by Associate II
  • 2728 Views
  • 3 replies
  • 0 kudos

Problem with sensor and freertos

Hi i have a problem. When i use a sensor with freertos and i put in the same task the function to read the value from the sensor and the osdelay() my task do one misuration and after do nothing. I print the value with the HAL_UART_Transmit.

TILEBOX - Proper charging behavior??

The User Manual states the RED flashing LED indicates the battery is charging but I'm not so sure about this. First, it appeared that I could not get any charging at all unless the the ON button was depressed for a few seconds. It also appears that...

0693W0000000B4lQAE.jpg 0693W0000000B4qQAE.jpg 0693W0000000B5KQAU.jpg
TJM by Senior II
  • 1398 Views
  • 3 replies
  • 0 kudos