Skip to main content
SAbid.2
Associate II
March 18, 2020
Question

How to reset the STEVAL-MKSBOX1V1 kit

  • March 18, 2020
  • 4 replies
  • 1111 views

Morning everybody, 

I have a STEVAL-MKSBOX1V1 kit, after flashing the microcontroller with an example of ST applicati I can't connect in bluetooth with my smartphone.

Could you tell me how to reset the STEVAL-MKSBOX1V1 program to factory default. 

I tried to load the BOOTLOADER.DFU on address 0x08000000 and the BLESENSOR.DFU on address 0x08004000 with DfuSeDemo but it still doesn't work, the blue LED flashes at the beginning and then goes off.  

Thank you  

    This topic has been closed for replies.

    4 replies

    Eleon BORLINI
    ST Employee
    March 19, 2020

    Hi @SAbid.2​ , which firmware are you trying to download on the ST.box? Did you already tried using the STM32Programmer tool as described at this link? You need to uninstall the DfUse drivers because they conflicts with the STM32Programmer tool ones. Btw, here attached the last factory FW in the .bin extension, if you need it. Regards

    SAbid.2
    SAbid.2Author
    Associate II
    March 19, 2020

    Hello, Eleon,

    This is the good firmware I am looking for "SensorTileBox", you are right for DfuSeDemo I just tried it with STM32CubeProgrammer and it works.

    Thanks for your help.

    Problem solved 

    SAbid.2
    SAbid.2Author
    Associate II
    March 19, 2020

    I'll get back to you, Mr. Eleon, (login problem ) 

    I have a connection problem with windows 7, I can't connect the SensorTileBox with my pc in windows 7 but it works with windows 10.

    Thanks

    Eleon BORLINI
    ST Employee
    March 20, 2020

    Hi @SAbid.2​ , I'll answer you on the new thread. Regards