LPS22DF for new design
Hello,Please the pressure sensor LPS22DF is it recommanded for a new design ?Thank you
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hello,Please the pressure sensor LPS22DF is it recommanded for a new design ?Thank you
Issue with Wrist Tilt Direction Detection on LSM6DS3TR-CHardware & Software Details:- Sensor: LSM6DS3TR-C- Platform: Arduino- Interface: I2CProblem Statement:We are working on detecting wrist tilt using the LSM6DS3TR-C sensor. While the tilt detectio...
Hello there, Are there any examples on how to use the inactivity feature of the lsm6dsv16x?I checked the github and I only see for waking up, but not the other way around. My goal is to set a device to sleep once there is no motion from imu. meaning...
I am using steval mkbox-pro with FP-SNS-DATALOG2 to get acceleration from the subway train.How can i remove the gravity effect in measurements from the LSM6DSV16X accelerometer?
Hello,I'm trying to calibrate the gyroscope of LSM6DSO MEMS but I don't really understand what describe the quality parameter in the MGT_state_t structure. I didn't find any information about it in the datasheet. Could you explain it to me ?I succeed...
Hi, I'm trying to use the LPS28DFW in one shot mode and there seems to be a discrepancy between the devices functionality and the application note.From an5758 section 3.2 - one shot mode: "One-shot mode has to be executed while the device is in power...
I configured both the accelerometer's and gyroscope's odr in asm330lhh to 6.667kHz, and used a FPGA to sample the acceleration and angular velocity as quickly as possible. The spi read start from 0x1E to 0x2F, which include both the ready bits and mo...
Hello To receive various Interrupt events how INT1 and INT2 Pins of LSM6ds3tr need to be connected with Microcontroller ?My assumption is INT1 and INT2 pins need to be connected with microcontroller GPIO pins and GPIO pins has to be configured to cat...
Hello all,I have a question regarding the MEMS audio sensor MP23DB01HP. I managed to read out the Soundlevel of the sensor. But I don't know how to interpret this value. My question is, how can I convert the soundlevel to obtain a corresponding value...
I want to recognise small movements with small acceleration.Which mode is best suited?Is it better to have a high sampling rate or a lower one?which filters?where do the large peaks (incorrect values) come from?But I can already recognise the acceler...