MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How does function LIS2HH12 reference and high pass filter?

I am developing a LIS2HH12 library and I have set all the posibles configurations. I don't understand why when I set the reference and active the high pass filter the output registers have a wrong value. I have did test and I see a strange behaviour,...

JMart.6 by Associate
  • 1314 Views
  • 1 replies
  • 0 kudos

Resolved! SensorTile.box schematics

Hi,I have a SensorTile.box from ST. But unfortunately there is no board schematics in the product resources part! I appreciate if some one help and let me know about it.Kind regards

Am1 by Associate
  • 3578 Views
  • 7 replies
  • 0 kudos

Why dose VL53L0 measure anormal value after a long time?

I use Arduino Uno and VL53L0 sensor appliction board.I measure a distance long time. (8h or more) But after some time(maybe after 1h or more), it measure distance but it is anormal.for example, normal status distance is 100-120mm, but after some tim...

SBae.2 by Associate
  • 900 Views
  • 0 replies
  • 0 kudos

HTS221 Temperature measuring

Hi,we are using HTS221TR. In the datasheet it is not clear what is the temperature range what the sensor can measure -40...85? +15°C....40?

Skew between samples of acceleration components in sensor IIS3DHHC

Hi guys,I would like know is there is any skew between the acceleration samples of each axe, i.e. ax, ay, az. In other words, if the acceleration components (ax, ay, az) are sampled at the same instant or in sequence. In this last case, I would like ...

Guille by Associate II
  • 4926 Views
  • 15 replies
  • 0 kudos

Software reset of VL6180X sensor.

Hello,I have multiple VL6180X sensors which are handled by i2c multiplexor. Once I power up the sensor and configure it I can get measurements, but after MCU reset or switch the power I cannot get new measurements anymore. And the same problem with a...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.