MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LPS25HBT boundary conditions for to design the cover

Hi, for a project, I have designed a PCB with the component LPS25HBT. We want to know if there are some technical recommendations about the sensor's boundary conditions.Will we have to design the cover with some distance between the sensor and the bo...

MRuiz.2 by Associate
  • 1410 Views
  • 2 replies
  • 0 kudos

H3LIS331DL Spurious Pulses On INT2 After Sleep To Wake

We have a project using the H3LIS331DL in a remote control to determine whether it has been dropped. One of the versions uses both INT1 and INT2 connections. The INT2 connection is used to turn a power supply on, which wakes up the micro (if it's not...

GFiel.8 by Associate II
  • 1427 Views
  • 2 replies
  • 0 kudos

Temperature reading from IIS3DWB

Can't figure out how to read or interpret the temperature reading from this MEM.I read the two register 20h and 21h and get an answer like this:RM20h02h14FFhThe very brief description in the spec sheet did not help me.Has anyone a hint?

How to configure mode 2?

Hello,I have STEVAL-MKI197V1 (lsm6dsox sensor) that I use to communicate over spi with my stm32 board, and getting accelerometer and gyro data. Now I want to connect to the i2c lines of STEVAL-MKI197V1 a magnetometer(lsm303agr). How to setup this mod...

suads by Associate III
  • 1350 Views
  • 6 replies
  • 0 kudos

Resolved! Generate .h file from .ucf Unico file ( LSM6DSOX )

Hi,​I'm working with the LSM6DSOX Machine Learning Core.I found the way to go from the data logs to the .ucf file, but I was wondering if there was an already available way to generate the corresponding .h file directly from Unico.I guess it would be...

SHadj.1 by Associate II
  • 1139 Views
  • 1 replies
  • 0 kudos

Resolved! How to use IKS01A2 with Nucleo WB55 on Unicleo-GUI?

Hi everybody,I've been trying to use an IKS01A2 mounted on a Nucleo WB55 in order to test a STEVAL-MKI197V1.I installed the drivers for virtual com and was able to do a blink test on the nucleo board (programming it with mbed compiler).However, I hav...

SHadj.1 by Associate II
  • 1643 Views
  • 2 replies
  • 0 kudos

What is the SA0 behaviour of LIS331DLH with floating SDO pin?

The LIS331DLH language is slightly different regarding the SA0 function, compared to the LIS331DL. The LIS331DL datasheet explicitly states that the SDO pin can be left floating and SA0 will be treated as a '1': "The slave address (SAD) associated w...

Pauline by Associate
  • 1349 Views
  • 1 replies
  • 0 kudos

Algorithm to calculate Vibration.

Hi,We are using LSM303AGR in our product and I am able to derive X, Y and Z axis G values.Now I want to calculate vibratio based on X, Y and Z values.What is the algorithm to calculate vibration using X, Y and Z values.Do you have any white paper or...

SWunn.1 by Associate
  • 1301 Views
  • 1 replies
  • 0 kudos