MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-MK1175V1/LIS2DE12 accel setup help

Hi, I'm using the LIS2DE12 as a motion detector for my nRF BLE product. I purchased the eval module (STEVAL-MKI175V1) and I'm trying to set it up over SPI from the nRF52 eval board. I followed the datasheet for the eval board and connected the basic ...

JChen.9 by Associate
  • 1382 Views
  • 1 replies
  • 0 kudos

Can we "deGauss" the LIS2MDL using register commands to reset the AMR when exposed to high field to remove large hard iron offsets? The MMC5983MA allows this, does the LIS2MDL?

We have noticed that several LIS2MDL have come back to us with very large magnetic field offsets. While these can be corrected by the usual offset calibration, the large offsets are due to exposure to a large magnetic field source somewhere in the en...

KWine by Senior
  • 933 Views
  • 2 replies
  • 0 kudos

Getting unexpected I2C Slave Address from a LSM9DS1 sensor and reading the wrong data from the register I just wrote in

I am using a STM32F030R8 nucleo board and a LSM9DS1 sensor. I'm just starting out learning about this stuff and I am having troubles reading from the sensor. Here are all the details about the problem I am having. I initialized the peripherals and th...

0693W000001qf6cQAA.png 0693W000001qf6hQAA.png 0693W000001qf6rQAA.png
ETerr.1 by Associate
  • 1770 Views
  • 2 replies
  • 0 kudos

STEVAL-STWINKT1 Data Stream

I recently acquired a STEAL-STWINKT1. I'm looking to be able to stream all the raw data from all the sensors (Including the ultrasonic FFT) at the maximum sample rate for a fixed amount of time, specified by me, into a csv file. I have tried many of ...

GSumm.1 by Associate II
  • 1347 Views
  • 3 replies
  • 0 kudos

MotionFX library floating point ABI

I'd like to use MotionFX library on STM32H7 together with FreeRTOS and STemWin Middlewares. I noticed that MotionFX has been compiled with -mfloat-abi=softfp, but others are prepared for -mfloat-abi=hard.Could you please prepare "hard" ABI version o...

sirius506 by Associate III
  • 2936 Views
  • 3 replies
  • 0 kudos

lsm6ds3 temperature compensation

Dear ST,As I tested with, the LSM6DS drifted follow temperature. As you can image bellow, red line is temperature and green is degree (was calculated from X, Y, Z )I'd like to confirm LSM6DS had internal temperature compensation? If NO, how to do it?...

0693W000000WIcWQAW.png
tpham.1 by Associate II
  • 3860 Views
  • 8 replies
  • 1 kudos