MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What is MMC_Input_t data_in.TimeStamp used for in MotionMC?

I have been using MotionMC and I think it has been working. My compass appears to reach calibration as it starts working as expected and the calibration value reaches 3 (the highest level?).However, I've noticed while looking over my code that I am ...

Rstua.1 by Senior
  • 870 Views
  • 3 replies
  • 0 kudos

lsm6ds3 Relative tilt function

I read AN4509.Single-axis tilt sensing is supported, but I can not tested it.1.Is Single-axis tilt sensing need gyroscope enable? Now gyroscope I disable it.2.Single-axis tilt sensing means I need disable other two-axis, remain only one sensing axis ...

ZhangTao by Associate II
  • 1573 Views
  • 3 replies
  • 0 kudos

Using interrupt as trigger to read LISD2W12's FIFO

Hi,I started working with LIS2DW12 trying to acquire simple data in pooling mode. I've done this wihtout any troubles using STM's mems drivers.Now, I'm trying to take this to a next level and I'm trying to work with LISDW12 FIFO's in interrupting mod...

MAndr.233 by Associate III
  • 2578 Views
  • 3 replies
  • 0 kudos

Question about the sign of raw sensor measurement

I have a problem when i read the AN4508 application notes.In the figure shown below, Xb, Yb and Zb are device body axes with a forward-right-down configuration. XA, YA and ZA are the accelerometer sensing axes.When sensor is placed still on the table...

0693W000001sakMQAQ.png 0693W000001sakvQAA.jpg 0693W000001salAQAQ.png
llau.1 by Associate
  • 1322 Views
  • 1 replies
  • 0 kudos

Resolved! LIS331DLH chips I got show wrong value under low temperature.

hello. I have a question about LIS331DLH. ​under low temperature, LIS331DLH chip z-axis shows wrong value.it is almost 100 difference between -10 degree and 22 degree. x,y axis is fine but only z axis is problem. every chip I got have same problem ex...

kdok .1 by Associate II
  • 1543 Views
  • 2 replies
  • 0 kudos

VL53L0X long range mode

I am using VL53l0x and I want to measure distances of 2 meters but I don't find the function to configure long range mode.

Mcabe.1 by Associate II
  • 768 Views
  • 0 replies
  • 0 kudos

Set LIS2DH12 in power down mode

Hello ST Community,My application involves nRF52 series processor which interfaces with LIS2DH12 via SPI and I am trying to reduce the power consumption as much as possible when the processor is in sleep mode. I understand that, as soon as power is a...

AB.4 by Associate II
  • 2119 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.