MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Trying to understand/use MotionGT library

Hello,I'm trying to calibrate the gyroscope of LSM6DSO MEMS but I don't really understand what describe the quality parameter in the MGT_state_t structure. I didn't find any information about it in the datasheet. Could you explain it to me ?I succeed...

AKE1_0-1740048512741.png AKE1_1-1740048710872.png
AKE1 by Associate II
  • 572 Views
  • 3 replies
  • 0 kudos

Resolved! lsm6dsl FIFO DATA misaligned.

hi,     we use one LSM6DSL sensor to read 3 axis acc FIFO data each second, but after some times, the FIFO out data become misaligned. the sensor setting is below:XL_ODR_26HZGyro disabled.FIFO ODR = 26HzFIFO threshold (water mark) = 128No decimationB...

cdong by Associate II
  • 872 Views
  • 6 replies
  • 1 kudos

Resolved! LPS28DFW one shot bit cleared before sample is ready?

Hi, I'm trying to use the LPS28DFW in one shot mode and there seems to be a discrepancy between the devices functionality and the application note.From an5758 section 3.2 - one shot mode: "One-shot mode has to be executed while the device is in power...

LSM6ds3tr Pin Connection with Microcontroller

Hello To receive various Interrupt events how INT1 and INT2 Pins of LSM6ds3tr need to be connected with Microcontroller ?My assumption is INT1 and INT2 pins need to be connected with microcontroller GPIO pins and GPIO pins has to be configured to cat...

Ajit1 by Associate
  • 404 Views
  • 1 replies
  • 0 kudos

How to calculate dBSPL from sound level

Hello all,I have a question regarding the MEMS audio sensor MP23DB01HP. I managed to read out the Soundlevel of the sensor. But I don't know how to interpret this value. My question is, how can I convert the soundlevel to obtain a corresponding value...

riyolu by Associate
  • 1759 Views
  • 4 replies
  • 0 kudos

LSM303AGRTR

With LSM303AGR to achieve the electronic compass function now 0-360 degrees can be obtained normally, has increased the calibration function; Why the uneven distribution 

leo12345678_0-1739840880586.png