MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DSV half precision error at ~180 degrees

Hi,We're using the lsm6dsv's SFLP algorithm to calculate IMU rotation. Recently however we noticed that the resulting rotation has big gaps at around the 180degree mark. We believe this is because of the half float precision, specifically because the...

1000000957.png
Gorbit99 by Associate III
  • 8338 Views
  • 29 replies
  • 15 kudos

Unable to calibrate LPS22DF

I am using a python script to update the One Point Calibaration register 1Ah, 1Bh. I put values in but the resultant reading of the normal pressure registers in 28h, 29h, 2Ah are way off. Does anyone have a script that might show exactly how it is do...

ism330dhcx ctrl3_c sw_reset I2C callback behavour

Hello awsome peaple of the ST fourms,I've been writing a program on the MB1551-U585AI1-D01 STM32U5 dev board, after getting DMA working and writing some AzureRTOS aware platform functions for the MEMS sensors on the board I have been very successful ...

Gravity problems on IIS3DWB

Hello community, I am an electronics engineer at the CNRS in Montpellier (France). I am currently working with the IIS3DWB vibration sensor When I use the LFP2 low-pass filter, the action of gravity is added to the measurements. I use the following d...

LPS25HBTR pressure reading decreasing over time

I have bought a MKI-165V1 to test LPS25HBTR,but I find that the pressure value is decreasing for a long time ,from 1014.117 to 1002.970 in an hour.It is not stable,the next is my initial code,what is the reason for ituint8_t data = 0x90;HAL_I2C_Mem_W...

2067 by Associate II
  • 2299 Views
  • 10 replies
  • 0 kudos

Resolved! LSM6DS3 + LIS3MDL calibration

Hello, Our teams is making a proof of concept about dead reckoning using a STM WESU board. The goal is to get pedestrian position onyl using ACC/GYR/MAG for a short period of time and small moves.First results in certains conditions are pretty good. ...

pierre63 by Associate II
  • 1622 Views
  • 7 replies
  • 1 kudos