MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Having problems getting compression to work on the LSM6DSOX

Trying to enable compression. I only see tags 0x01 and 0x02, none of the compression tags.bellow is my reg inits.#define IMU_READ_BIT 0x80   #define EMB_FUNC_EN_B 0x05 #define FIFO_CTRL1 0x07 #define FIFO_CTRL2 0x08 #define FIF...

DFors.1 by Associate II
  • 3704 Views
  • 8 replies
  • 0 kudos

Application example for step counter using LIS2DS12

Hello ST community,I would like to know if there are examples available for configuring LIS2DS12 for pedometer applications. I see that the Github examples (https://github.com/STMicroelectronics/STMems_Standard_C_drivers/tree/master/lis2ds12_STdC/exa...

AB.4 by Associate II
  • 1316 Views
  • 4 replies
  • 0 kudos

Does Sensortile.box support mesh ble networks?

Hi everyone, I am trying to develop a mesh network using many sensortile.box, is it possilbe to use STSW-BNRG-Mesh with Sensortile.box? If it is not possible how is there any SDK available for Mesh networks using Sensortile.Box?Thank you.

LMaga.2 by Associate
  • 980 Views
  • 1 replies
  • 0 kudos

SensorTile.box connection problem

Helloi am trying to program my sensortile.box in pro mode. I have everything I need to be able to upload binary files (JTAG adapter, ST-LinkV2) but I encounter this error. Can anyone help me?

0693W000003Bhv9QAC.png
GCele.1 by Associate II
  • 1073 Views
  • 1 replies
  • 0 kudos

How to light a LED with PNUCLEO VL6180X

Hello I would like to have your help I use the vl6180X sensor for a proximity detection, on PNUCLEO, I want to know how to turn on an LED, I programmed the thresholds of my interruption and I would like to turn on an LED on the gpio1 the time of inte...

MSAMB.1 by Associate III
  • 1241 Views
  • 1 replies
  • 0 kudos

Resolved! I am facing issue while programming STWINKT1 board using stm32cube ide

I am previously using STM32CubeIde version 1.3.0 and i am able to programme the STWINKT1 development board successfully. while i am debugging suddenly my laptop crashed and when i power on it again now i am getting error.So i uninstall version and do...

0693W000002lEPMQA2.png 0693W000002lEPWQA2.png 0693W000002lEQjQAM.png
karan by Associate III
  • 1628 Views
  • 2 replies
  • 0 kudos

Does the INTERNAL_FREQ_FINE register of ASM330LHH indicate that there is a frequency deviation? In this case, how should it be used under the standard time interval algorithm requirements?

Hello, may I ask whether the INTERNAL_FREQ_FINE register was written before delivery?Can it be understood that the actual data frequency of each ASM330LHH IC is different?My project will use many same sensors to collect acceleration and gyroscope at ...

wb.2 by Associate
  • 966 Views
  • 2 replies
  • 0 kudos