User Activity

Hi,I've tried to configure the DREADY to INT1 and read the output registers. I believe I'm making some mistake in the configuration as I observed that I'm able to read the OUT registers when I using the polling method. I've tried using the ST MEMS C ...
Hi,​I'm trying to interface a nrf52840 DK with a LIS2DW12. I'm using the ST-Eval board for the IMU. ​I'm able to read the WHO_AM_I register and it gives the correct value(0x44). I tried setting the IMU to 100Hz and the high performance mode. When i t...
Hi,I have a MCU connected to a LSM6DSM using I2C with 1k pullups. I measured the average current consumption with the MCU and the LSM6DSM powered up but with the I2C lines physically disconnected. The current consumption was around 20uA.Once I connec...
Hi,I'm using a LSM6DSM to detect periods of inactivity and put a MCU to sleep. Similarly, it uses the activity interrupt to wake the MCU. I observed an average current consumption of ~0.7 mA when configured to check for inactivity(Gyro enabled and OD...
Hi,I am using the LSM6DS3 with I2C at 400 kHZ. I would like to know the pin capacitance value so as to calculate the value of the required pull up resistors. I was unable to find this in the data sheet.Thanks
Kudos from