MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Strange yaw behavior in using MotionFx Library?

I am trying to feed the sensor readings (gyro in dps and acceleration in G) to the MotionFx library, correctly specify the orientation (verified by ST local FAE) for 6X calculation.At beginning I put the PCB on table, after power on and initializatio...

MChen.10 by Associate II
  • 6140 Views
  • 14 replies
  • 0 kudos

Resolved! ERROR VL53L0X

Hello,I'm using the VL53L0X's API when I open the example project of rangewithsatellite and I compile the main programme, these error message is displaying to the console someone can tell me what should I do? Thank you this pictures show the error co...

MSAMB.1 by Associate III
  • 3572 Views
  • 5 replies
  • 0 kudos

Resolved! Self test on the LIS2DE12TR

Hello,I am working on a project where I have to interface the LIS2DE12TR Accelerometer via I2C interface with TI cc2652 chip. As a start I wanted to verify the hardware functionality. In the datasheet it is mentioned of a Self-Test Mode of operation....

SShan.11 by Associate II
  • 9458 Views
  • 20 replies
  • 1 kudos

Resolved! ISM330DLC: Interrupt on Linux

Hello,I'm try using ISM330DLC connect to Linux OS on board IMX8MP via I2CLinux supported driver for this device (iio/imu/st_lsm6dsx); I added to dts file as below:&i2c5 { clock-frequency = <100000>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl...

Tdo.1 by Associate II
  • 7425 Views
  • 6 replies
  • 0 kudos

Resolved! I am using the example project MEMSMIC1 in order to stream audio to host PC. But it is not working beside the following configuration: 2 channels, 16000 sample rate.

When I am changing the number of channels to 1 channel.it is recognized by the windows driver, but the"advanced" TAB is disappear (unlike 2 channels configuration). Did someone faced with this kind problem? Do I missedsomething? of course, audacity d...

AA.10 by Associate III
  • 2666 Views
  • 10 replies
  • 0 kudos

Sensortile box firmware

Which firmware version​ should be on sensortile box? Any other recommendations is much appreciated.​I am having issues with 2 of 2 sensortile boxes I received yesterday​. All interactions have been with Android st ble app. No response from one and...

MDupu.1 by Associate II
  • 3609 Views
  • 10 replies
  • 0 kudos

Synchronization of multiple ISM330DHCX

Hello,I need to use dual MEMS (ISM330DHCX) and MCU in my application for redundancy. Each MEMS is connected to a different MCU with independent supply. The data collected from sensors will be crossed checked if within a predefined tolerance. I think ...

JVinc.1 by Associate III
  • 5961 Views
  • 14 replies
  • 0 kudos