MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSM9DS1 - Understanding gyro configuration

I have an application using an LSM9DS1 sensor, where I'm only interested in ready gyro values in order to determine angular velocity around the Z-axis.Looking at the datasheet in page 45, table 46, what does it mean the cutoff frequency in that table...

PRebo.1 by Associate II
  • 3734 Views
  • 5 replies
  • 0 kudos

Resolved! bug report [cubeMX] Makefile gen

i'm a linux user, so i use cubeMX gen a code framework with project type: Makefilesnow, i try to use x-mems lib, the makefile is miss a ":" that lead "make" command error.after add the colon, seems goodFYI

0693W000004I5N2QAK.png
MMa.1893 by Associate III
  • 1541 Views
  • 1 replies
  • 0 kudos

Please provide guidance on VL53L3 calibration.

The "VL53LX API Specification" 1.1.4.2352 lists 13 "calibration functions" but provides little guidance on what they do and when they should be called. The VL53L3 data sheet says calibration is required and "The detailed procedure is provided in the ...

charles23 by Associate III
  • 3733 Views
  • 9 replies
  • 1 kudos

Resolved! LIS2DE substitute

Hi,We've got an old design with an LIS2DE sensor, but it is obsolete. Is there any part compatible pin-to-pin? Thanks in advanceBest regards,Manuel