2024-12-06 1:27 AM
Hello community,
I have an application where I want to implement STHS34PF80 for detecting people PRESENCE and MOTION with a range of 3 to 4 meters. In the Datasheet it is stated that it is possible without using extra lenses. Although, I am struggling to find the best config to have a good recognition with more than 1,5m.
- What would be the step-by-step to make the sensor run in 4 meters range?
- Could someone give me an example config for THRESHOLD, HYSTERESIS, LPF, ODR and AVG?
2024-12-06 5:20 AM
Hi @Marcelo_GWA ,
For the configuration of the sensor and of the presence detection algorithm, we suggest to follow the procedure described in the AN5867.