MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! IMU with or withour magnetometer

HiI am not an IMU expert. My current task is to upgrade an old board which used LSM6DSL(gyro abd accelerometer ) and lsm303agr(Magnetometer) to caliculate orientation of a human head.As far as I can see LSM6DSV would be providing orientation data wit...

MK..1 by Associate III
  • 802 Views
  • 2 replies
  • 0 kudos

Resolved! ISM330DHCX Incorrect FIFO data / correct direct reading

[EDIT 03/04/25 09:15:35 AM] Well, it appears that, as usual, the real issue was sitting right in front of the keyboard… and could have been solved with a good old ‘Read The Freaking Manual.’ My deepest apologies for this classic case of user error! :...

Marconfr by Associate
  • 536 Views
  • 2 replies
  • 0 kudos

Is it possible to use Sensortile.box Pro with Pi Pico W?

Would it be possible to connect and send sensor data to a Pi Pico W from the STEVAL-MKBOXPRO? I’m looking for a way to connect them together via Bluetooth but a wired connection would be alright too. I have connected a Pico to the sensortile box via ...

spi1 by Associate
  • 412 Views
  • 2 replies
  • 0 kudos

Is my ASM330LHH imu sensor spi code correct?

I want to read acc and gyro data from my ASM330LHH sensor with spi communication, but I can't try the code because I don't have a sensor at the moment, can you take a look at the code, is there anything wrong or missing?(I selected the SPI_CS pin as ...

lis2dw12 linux driver difference

there are two kinds of linux driver for lis2dw12 in LIS2DW12 - 3轴MEMS加速度计,超低功耗,可配置单/双击识别,自由落体,唤醒,纵向/横向,6D/4D方向检测 - 意法半导体STMicroelectronics which is LinuxDriverIIO and LinuxDriverInput,1.what's the difference, which should we use, Do you have an appli...

xuehua by Associate
  • 480 Views
  • 1 replies
  • 0 kudos

Resolved! The differences between the IIS2DLPC and LIS2DW12

Could you tell me the differences between the IIS2DLPC and LIS2DW12?According to the reference URL, are there any differences between these two devices other than product longevity and guaranteed parameter values? I am particularly interested in whet...

MYabe.1 by Associate
  • 533 Views
  • 1 replies
  • 2 kudos

Resolved! SensorTile.box PRO : Record human activity and pedometer

Hello, @Andrea VITALI,After using the WESU board (https://community.st.com/t5/mems-sensors/lsm6ds3-lis3mdl-calibration/td-p/762534)we decided to move forward with the sensor tile box PRO. We want to record human activity recognition and pedometer inf...

pierre63 by Associate II
  • 3955 Views
  • 11 replies
  • 2 kudos

Resolved! SPI NSS-Signal by Hardware, using IIS3DWB on an STM32L432 MCU

Hello!We are developing with the sensor IIS3DWB. I am able to interface it by spi like mentioned in st's github example, and I'm able to use st's platform independend c-drivers. It works fine, I get Acceleration, Temperature, device-ID...In that exam...

PR.4 by Associate II
  • 1476 Views
  • 3 replies
  • 0 kudos

ASM330LHH gyro anti-pre-ADC aliasing filter

Hello, we are using the ASM330LHH in our product and are doing some bandwidth testing and trying to model the gyro channel behavior. Our settings are ODR = 6667Hz, LPF1 bandwidth = 470, LPF2 =3333Hz. Looking at the data sheet "Gyroscope filtering cha...

tjbh by Associate
  • 853 Views
  • 3 replies
  • 0 kudos