MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What are the necessary Configuration and Calculations for LSM9DS1?

Hi Team.We are using LSM9DS1 with MCU (S32K146) via I2C. We have tried enabling the acc and gyro with CTRL_REG1_G and CTRL_REG6_XL .We can able to read the Who am I register properly. But the data output registers of acc/gyro are giving different val...

LG.2 by Associate
  • 1666 Views
  • 4 replies
  • 0 kudos

Resolved! LPS33HW Temperature absolute accuracy

Temperature absolute accuracy. This parameter was not found in the datasheet.Of the 15 sensors tested, the temperature ​difference was 5 degrees.What ​temperature absolute accuracy should be?

PSoko.1 by Associate II
  • 1653 Views
  • 5 replies
  • 0 kudos

I tried to install the GUI en.STSW-IMG004 to run my EvalBoard with VL53L1x. But the insatllation end with Error Massage 1721.

Hello everybody,I tried to install the GUI en.STSW-IMG004 to run my EvalBoard with VL53L1x. But the insatllation end with Error Massage 1721 (see attached). I ried it also on a second Hardware with the same result. What did I make wrong? Regards Dani...

DPalm.1 by Associate
  • 1545 Views
  • 4 replies
  • 0 kudos

How to detect angular movement and wake up LIS2DW12

Hi, I have an LIS2DW12 fitted to a STEVAL-MKI179V1 board. I have it connected to a microcontroller programmed to set an interrupt pin on wake up as per DT0098. The interrupt pin goes high with a light tap in the xy or z axis. However I want it to det...

DSqui by Associate II
  • 2108 Views
  • 5 replies
  • 0 kudos