MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS2DH register details missing

Hi there,I was working on the LIS2DH for one of our applications, and found that there are some details missing in the datasheet (Doc ID 022516 Rev 1), enlisted below:1- The bits HPCF2 - HPCF1 in the CTRL_REG2 (21h) corresponding to the high pass fil...

Smalik by Associate II
  • 1150 Views
  • 4 replies
  • 0 kudos

Resolved! SensorTile MEMS Audio stream to Unix-like OS (Raspbian)

I am exploring the SensorTile (STEVAL-STLKT01V1) and would like to capture Audio recordings on a Unix OS (namely Raspbian). I have looked through the documentation here and the option to save audio to SD card is not ideal for my application, neither...

Resolved! VL6180X INTERRUPT TO GPIO1

Hello,I am using a PNUCLEO VL6180X and I would like to drive my LED from the GPIO1 interrupt output only this output as shown in the diagrams above is always at 1 and it goes to 0 only for a few nanoseconds; I would like to have an interrupt signal o...

MSAMB.1 by Associate III
  • 6091 Views
  • 8 replies
  • 0 kudos

Support for Unicleo-GUI

Hi Team,Dear TeamGone through the user manual, refer the below linkhttps://www.st.com/content/ccc/resource/technical/document/user_manual/group0/b9/d0/7c/c5/a8/55/4c/bc/DM00337036/files/DM00337036.pdf/jcr:content/translations/en.DM00337036.pdfAlso fi...

SS_135 by Associate II
  • 2687 Views
  • 6 replies
  • 0 kudos

Is there a demo for VL53L3CX that help me to understand how to manage different ToFs together? Something similar to the MultiRangingSensor demo for VL53L1X.

Hi, my name is Vincenzo. I am working with the ToF VL53L3CX. Lately I wrote some applications to make 6 sensors work. At first I thought that the applications were working well, but now I realized that if I set too high timing budgets I had a perform...

VNava by Associate III
  • 4166 Views
  • 10 replies
  • 0 kudos

Resolved! My code is working as it wishes

Hi everybody , I am not sure about am I writing to the true title but anyways I am asking. I am trying to read data from LSM9DS1 sparkfun IMU sensor using HAL i2c with STM32F4 discovery board. I was succesful and I was getting datas, then something h...

MDoğr.1 by Associate II
  • 2261 Views
  • 3 replies
  • 0 kudos

Resolved! Gadget position sensor

Hi, our customer is in search for a economical solution for a gadget posistion sensor, that senses 2 positions: the gadget is in standing or in laying positions. What can we suggest?

LSM6DSM: Increase in current draw once I2C lines are connected

Hi,I have a MCU connected to a LSM6DSM using I2C with 1k pullups. I measured the average current consumption with the MCU and the LSM6DSM powered up but with the I2C lines physically disconnected. The current consumption was around 20uA.Once I connec...

GTS.1 by Associate III
  • 2615 Views
  • 6 replies
  • 0 kudos

LIS2DH taking 100-120uA in idle state after a power cycle

I am using LIS2DH in I2C mode. After power cycle, the IC consumes almost 100-120 uA. Upon removing the IC current drops to 30 uA so clearly it is the IC that is consuming the power.After startup, I am resetting the IC, blocking the data (0x80 in REG ...

PK.1 by Associate II
  • 4508 Views
  • 10 replies
  • 0 kudos

VL53L1 Ranging instability in strong ambient light

Hi,I'm trying to use multiple VL53L1X sensors to detect objects. I successfully interfaced them with a Raspberry Pi 4B, and tried to tune a bunch of parameters to get good detection.When the sensors point to an object, within the sensor range (0.4 - ...

THilt.1 by Associate II
  • 3683 Views
  • 5 replies
  • 0 kudos