cancel
Showing results for 
Search instead for 
Did you mean: 

How do I determine what the top marking is for the device LPS25HBTR so as to verify that we have the correct component when scanning these at AOI?

JDows
Associate

We have devices marked 8198 and 7298, we are thinking these may be date codes and no the component part number code.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Hi @JDows​ ,

If the information was useful for you, please click on Select as Best if my reply fully solves your problem or answers your question to help future community users with the same question.

Thanks,

-Eleon

View solution in original post

2 REPLIES 2
Eleon BORLINI
ST Employee

Hi @JDows​ 

you should see 3 numbers and 1 letter in column, below the dot marker.

For example: ° 620B, or, in column:

°

8

1

9

B (not "8")

  • 8 is the year of production, meaning 2018
  • 19 is the week of the production year
  • B is the part number marker, the "B" in bold, LPS25HBTR

-Eleon

Eleon BORLINI
ST Employee

Hi @JDows​ ,

If the information was useful for you, please click on Select as Best if my reply fully solves your problem or answers your question to help future community users with the same question.

Thanks,

-Eleon