MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Coding sensor fusion application on Sensortile.box

In order to do bench-marking of the work of sensor fusion I wanted to create a code application to test it out. The one provided as a part of the phone app doesnt work reliably, also wanted to code it myself. I was checking intro provided on the webs...

VRakc.1 by Associate II
  • 2497 Views
  • 4 replies
  • 0 kudos

How do I initial CS43L22 on STM32F407G?

Hi,I tried couple to run my code, but I can't just hear any noise or beep. I am very new to this.One issue that I found is SPI3->DR is not receiving anything during debugging.Here is my code and correct me,#include <mbed.h>#include<I2C.h>#include <st...

BC.1 by Associate
  • 1581 Views
  • 1 replies
  • 0 kudos

H3LIS200DL doesn't generate an interrupt

I am trying to get an interrupt when exceeds the limit (for test, 1g), but couldn't see any changes on INT1 line.I have configured H3LIS200DL INT1 (INT1_THS is 0x01, INT1_DURATION is 0x03, INT1_CFG is 0x63). I am getting OUT_X, OUT_Y, OUT_Z between -...

honestech by Associate II
  • 1157 Views
  • 1 replies
  • 0 kudos

Making a demo for VL53L3CX to manage different ToFs together using interrupt? I found MultiRangingSensor demo for VL53L1X and trying to modify it to work for VL53L3CX ,I have noticed that the code works for sensors sequentially!

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) { if (GPIO_Pin==VL53L1X_INT_Pin) { IntCount++; }   }   /* USER CODE END 0 */   int main(void) { /* USER CODE BEGIN 1 */   uint8_t byteData; uint16_t wordData; uint8_t ToFSensor =1; // 0...

HElni.1 by Associate II
  • 2816 Views
  • 4 replies
  • 0 kudos

LSM6DSM/LSM6DSR gyro angular random walk and bias stability

Our commercial product currently uses the LSM6DSM. We would like to upgrade to a lower noise accel/gyro. The ISM330DHCX has a gyro bias stability indicated in the data sheet at 3 degrees per hour, which seems about half the value for competing gyros....

KWine by Senior
  • 1391 Views
  • 1 replies
  • 0 kudos

Resolved! Precision achievable with LSM9DS1 gyro ?

In my project I have a LSM9DS1 with the purpose of measuring angular speed on the XY plane.I'm using for calibration a reference platter spinning at a constant 33rpm, and the code handling the gyro removes a previously measured 0-state offset and de...

PRebo.1 by Associate II
  • 1687 Views
  • 1 replies
  • 0 kudos

Resolved! Algobuilder flexible number of properties

Hi!I am using Algobuilder and I tried to use a flexible number of properties (like for example in the "Graph"). Although undocumented, I saw in the library for the display that there are <DisplayDependency> and <DisplayCondition> tags. I tried to use...

DWind.1 by Associate III
  • 1419 Views
  • 1 replies
  • 1 kudos