cancel
Showing results for 
Search instead for 
Did you mean: 

H3LIS200DL doesn't generate an interrupt

honestech
Associate II

I am trying to get an interrupt when exceeds the limit (for test, 1g), but couldn't see any changes on INT1 line.

I have configured H3LIS200DL INT1 (INT1_THS is 0x01, INT1_DURATION is 0x03, INT1_CFG is 0x63). I am getting OUT_X, OUT_Y, OUT_Z between -2 and 0.

The sensor datasheet describes 7 bit threshold, so I think 1 LSB is 100/127g.

I am not sure what I am missing. Any help would be appreciated.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
honestech
Associate II

I have tried with LIRx of CTRL_REG3. When LIR1 sets to 1, reading INT1_SRC generates interrupt even if doesn't reach threshold (tested with 100g). But without reading INT1_SRC, I couldn't see any interrupt pulse on INT1 line. The interrupt interval is same to reading interval.

What I might be wrong or have to set anything?

Does anyone can explain this?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.