Skip to main content
PRebo.1
Associate II
November 20, 2020
Solved

Precision achievable with LSM9DS1 gyro ?

  • November 20, 2020
  • 1 reply
  • 1115 views

In my project I have a LSM9DS1 with the purpose of measuring angular speed on the XY plane.

I'm using for calibration a reference platter spinning at a constant 33rpm, and the code handling the gyro removes a previously measured 0-state offset and denoises the reading using moving averages.

However, whenever I start it, I seldom get the same average readings. They might difer (the average) by +/- 0.02 DPS. Is this the precision limit, or something better can be achieved ?

This topic has been closed for replies.
Best answer by Eleon BORLINI

Hi @PRebo.1​ ,

the precision achievable with the LSM9DS1 gyro are defined in the datasheet, p.12:

0693W000005CJjxQAG.pngThis mean that, from a theoretical point of view, once you have compensated (or filtered) the angular rate typical zero-rate level, you are able to resolve your running angular speed with about 10 mdps resolution in the FS = ±245 dps case. So +/-0.02 dps is not so distant from the actual theoretical limit (about 0.1 dps), and is a probable value, considering additional noise. You can of course average in time, especially increasing the ODR (max = 952 Hz) so that you have more point for averaging in the same time frame.

Please note however that the LSM9DS1 gyroscope is not the best-in-class device as regards the gyroscope: the LSM6DSO(X), for example, is able to run at FS = ±125 dps, reducing the by a factor of 2 the minimum detectable signal, i.e. the precision limit.

-Eleon

1 reply

Eleon BORLINI
Eleon BORLINIBest answer
ST Employee
November 23, 2020

Hi @PRebo.1​ ,

the precision achievable with the LSM9DS1 gyro are defined in the datasheet, p.12:

0693W000005CJjxQAG.pngThis mean that, from a theoretical point of view, once you have compensated (or filtered) the angular rate typical zero-rate level, you are able to resolve your running angular speed with about 10 mdps resolution in the FS = ±245 dps case. So +/-0.02 dps is not so distant from the actual theoretical limit (about 0.1 dps), and is a probable value, considering additional noise. You can of course average in time, especially increasing the ODR (max = 952 Hz) so that you have more point for averaging in the same time frame.

Please note however that the LSM9DS1 gyroscope is not the best-in-class device as regards the gyroscope: the LSM6DSO(X), for example, is able to run at FS = ±125 dps, reducing the by a factor of 2 the minimum detectable signal, i.e. the precision limit.

-Eleon