MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS2DH12 self test query

Hello,We are using LIS2DH12 sensor in our product. We are following the self test procedure mentioned in AN 5005 Section-12.We have confusion about how to use the raw data from OUT_L and OUT_H of each axis.(1) Do we need to convert raw data into grav...

0693W000007Bz5WQAS.png
kghin.1 by Associate II
  • 2824 Views
  • 3 replies
  • 0 kudos

Algobuilder with ArmCortex M0+ Nucleo

Hi!We are using AlgoBuilder with the NUCLEO-L476RG and it is working pretty nice. We wanted to try out our AlgoBuilder application on an Arm Cortex M0+ board to evaluate power consumption and behaviour. From what I saw from the documentation it seems...

DWind.1 by Associate III
  • 1560 Views
  • 1 replies
  • 0 kudos

Resolved! What is the advanced feature of the pull up at pin SA0 of IIS2DH?

We discovered that the SA0 Input of the IIS2DH of your accelerometers has a very high pull up current.The pull up is about 40 kOhm at IIC adress select line input. If engineers will use two IIS2DH in there design.Than the IIS2DH at adres 0x18, mea...

MVerm.11 by Associate
  • 1933 Views
  • 3 replies
  • 0 kudos

I am using the LIS2DH12 and get expected values in normal mode. When changing to high res mode the scaling is not as expected.

FS=11, BLE=0, LPen=0, HR=0 (10-bit normal mode, +/-16g FS). I expect the sensitivity to be 48mg/digit, and sure enough, if I right-align my 10-bit value and divide by 48 I get a value of about 1054 on the z-axis.When I set HR=1, no other changes, I e...

CLaw.1 by Associate II
  • 2488 Views
  • 6 replies
  • 0 kudos

Resolved! H3LIS331DL precision / default calibration

Without any move, my H3LIS331DL on a MKI153V1 kit, and read from and STM32L4 MCU, gives values around X=1,5 / Y=2 / Z=3 G at 200g full scale.Is that "Zero Offset" normal ?Should I do anything to get values closer from 0 / 0 / 1

PGoud by Associate III
  • 1894 Views
  • 2 replies
  • 0 kudos

Less number of samples collected than the sample rate used

I am using Lis3DSH at 1600 sample rate . I am using I2C at frequency 250Hz for communication with sensor.If I want to capture 3 seconds data(4800 samples), the actual time taken to complete this procedure is more than 3 seconds, which means overrun i...

AK.08 by Associate III
  • 4123 Views
  • 8 replies
  • 0 kudos