User Activity

Is it really possible to configure H3LIS331DL to fire an interrupt (a pulse) for each DataReady ?I've never succeded in doing that, It seems to be always mandatory to read Acceleration to "release" the interrupt line, hence being able to have a new i...
Hello,Is there any ressource describing the consumption during 10Hz Low-power mode ?On my side I think I can see little peaks each 100ms then one litle larger peak each 2 seconds.Is that the normal behavior ?Is it possible to find a typical consumpti...
My configuration is:FS: 200g, Threshold interrupt activated for hieZ,hieY,hieZ, Threshold value 1 (ie about 1,6G at FS 200G)High pass filter set on OUTPUT and INT1Then I loop, reading int1 src register and 3 axes accelerationthey varie on each channe...
Hello,I can succesfully have ready (DRDY) under interrupt (INT1) at low or normal power vfrequencies. Cool.BUT I do not success in using threshold and duration.Can anyone, can give me the correct configuration to do this:Get an INT1 interrupt each ti...
I've got erratic behavior of access to H3LIS331DL sensor from my MCU when STOP2 mode is set. It seems that sometimes, the Interrupt ( INT1 on DRDY) received from theH3LIS331 is not, or very lately processed (maybe after wake up from other reason). I...