MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS2DW12 shared SDI and CLK lines cause current leaks

Hello!We have developed two types of custom boards, with two different MCUs. On board number 1, each peripheral unit has its own SPI lines dedicated to it. On board number 2, the number of GPIOs has decreased, so we decided that the CLK and MOSI (SDI...

APipm.1 by Associate II
  • 3742 Views
  • 6 replies
  • 0 kudos

What is the best way to make the VL53L0X / VL53L1X water resistant? Will they still work when encapsulated in transparent epoxy?

Hi,I'm asked to design an industrial device to detect objects within about 1 meter. The devices will be placed in a very harsh environment (moister/water) so we want to encapsulate the PCB with sensors in transparent epoxy. I have looked at this vide...

mrWheel by Associate
  • 3097 Views
  • 2 replies
  • 0 kudos

MotionTL calibration fails

Hi,I am currently trying to calibrate a LSM6DSL using the MotionTL calibration but it keeps failing. There must be something I am doing wrong, but I have not been able to find it while comparing my code to the mems examples. MTL_acc_cal_t calibratio...

KHeye.1 by Associate III
  • 2496 Views
  • 5 replies
  • 0 kudos

Resolved! LSM6DSO vs LSM6DSOX

Is the only difference between the two that LSM6DSOX has the machine-learning core (MLC)?In other words, are the 2 parts interchangeable when the MLC is not used?

Resolved! Hello Experts of ST community, I have mems mic and stm32f4xx nucleo board and collected the pcm format data in a log files. Now my query is how to convert them into .WAV format ? and How to validate the the values are exactly accurate?

Can someone help me figuring out how do we conclude the obtain pcm values are accurate and can there be any references to validate it and test it back?Any suggestions please help?

SG.4 by Associate II
  • 1248 Views
  • 1 replies
  • 0 kudos

SM32Cube IDE MEMS1

Hello ST MEMS Community.I recently switched to use STM32 CubeMX IDE and I really like it .I would to utilize full power of the IDE and would like to use MEMS sensor for my application. I have installed X-CUBE MEMS pack.I did see multiple device avai...

IB.1 by Associate III
  • 2530 Views
  • 5 replies
  • 0 kudos

Resolved! Data corruption with PDM Microphone

Hello, I am using a MEMS PDM microphone and reading it in using I2S. The following parameters are set in my I2S and PDM configurations.hi2s3.Instance = SPI3; hi2s3.Init.Mode = I2S_MODE_MASTER_RX; hi2s3.Init.Standard = I2S_STANDARD_MSB; hi2s3.I...

kcire L. by Associate III
  • 4870 Views
  • 11 replies
  • 0 kudos

How do you calculate the tri-axis(mag, access, gyro or fusion) outputs (+/- 1over 180 degrees) to accurately cover 360 degrees in code and what are those conversion. So that one physical rotation of the device equals 360 degrees exactly.

How do you calculate the tri-axis(mag, access, gyro or fusion) outputs (+/- 1over 180 degrees) to accurately cover 360 degrees in code and what are those conversion. So that one physical rotation of the device equals 360 degrees exactly. Currently us...

CTone.1 by Associate
  • 1416 Views
  • 1 replies
  • 0 kudos

[Webinar] Would you like to learn more about Content Level Management Applications using ST FlightSense Time-of-Flight Sensors?

Join our 1-hour webinar to discover how ST Time-of-Flight proximity and ranging sensors can beat content level monitoring challenges Tuesday, March 2nd, 2021 | 3:00 pm CETYou will learn:The benefits ToF sensors in content level management application...

0693W000007ZigEQAS.png

Resolved! MotionFX "nan" values after a while on Discovery kit IoT node

Hi,I'm testing the MotionFX library with the Discovery Kit IoT node [B-L4S5I-IOT01-A] and I have a problem: randomly the sensor fusion algorithm "explodes" and I can only get only "nan" values for all the `MFX_MagCal_output_t` values, Gyro Biases inc...