MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I'm using the LIS3DH. Do I need to provide a 90 mS delay between configuration of CTRL_REG1 and reading the OUT registers or the FIFO to insure stable output ?

I'm using the LIS3DH. The Application Note AN3308 specifies a 90 mS delay time between configuration and reading data in the suggested procedure for performing a self test, (p57 of DocID18198 Rev 3). The delay is, "... for stable output".  Once ODR i...

JMatt by Associate II
  • 1502 Views
  • 2 replies
  • 0 kudos

Resolved! LIS2DW12 Accelerometer tilt angle detection

Hi,I am using LIS2DW12 Accelerometer for tilt angle detectionIs it possible to detect the tilt angle(A and B) in both directions as shown in figure and trigger the interrupt event in wakeup interrupt mode?It is possible in 6d orientation mode, but I ...

0693W000007ZujeQAC.png
MIR.1 by Associate II
  • 3769 Views
  • 7 replies
  • 0 kudos

Resolved! LSM6DSM Sourcing Difficulties

Hi, so basically I am looking to source the IMU LSM6DSM. I see that it is out of stock almost everywhere. Is this device being discontinued? Why is it so hard to purchase?If you have a more in-stock variant, with the same pinout, please let me know. ...

CMarc.3 by Associate
  • 1677 Views
  • 3 replies
  • 0 kudos

Low throughput reading multiple VL53L1X

I'm programming a sensor array composed of 12 VL53L1X ToF sensors, connected to an STM32F427 chip through a single I²C bus. Measurement and inter-measurement times are set to 30 and 40 milliseconds respectively across all sensors. Sensors are queried...

HPerr.2 by Associate
  • 1406 Views
  • 1 replies
  • 0 kudos

Accelerometers in time-interleaving mode: problems and solutions

Hello!I have multiple LIS2DS12 accelerometers; according datasheet, it is possible to get data rate high as 3200 and even 6400 Hz. In both cases there are built-in filter with 1420 or 2840 Hz cutt-off frequency. As this accelerometer have internal mu...

Dfsd .1 by Associate
  • 1188 Views
  • 1 replies
  • 0 kudos

LIS3DE substitute

Hi, what is the natural replacement for the obsolete LIS3DE?Is there a model pin to pin compatible and software compatible?Thanks.

pb.11 by Associate
  • 1117 Views
  • 1 replies
  • 1 kudos