MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS2DW12 Accelerometer tilt angle detection

Hi,I am using LIS2DW12 Accelerometer for tilt angle detectionIs it possible to detect the tilt angle(A and B) in both directions as shown in figure and trigger the interrupt event in wakeup interrupt mode?It is possible in 6d orientation mode, but I ...

0693W000007ZujeQAC.png
MIR.1 by Associate II
  • 3658 Views
  • 7 replies
  • 0 kudos

Resolved! LSM6DSM Sourcing Difficulties

Hi, so basically I am looking to source the IMU LSM6DSM. I see that it is out of stock almost everywhere. Is this device being discontinued? Why is it so hard to purchase?If you have a more in-stock variant, with the same pinout, please let me know. ...

CMarc.3 by Associate
  • 1628 Views
  • 3 replies
  • 0 kudos

Low throughput reading multiple VL53L1X

I'm programming a sensor array composed of 12 VL53L1X ToF sensors, connected to an STM32F427 chip through a single I²C bus. Measurement and inter-measurement times are set to 30 and 40 milliseconds respectively across all sensors. Sensors are queried...

HPerr.2 by Associate
  • 1396 Views
  • 1 replies
  • 0 kudos

Accelerometers in time-interleaving mode: problems and solutions

Hello!I have multiple LIS2DS12 accelerometers; according datasheet, it is possible to get data rate high as 3200 and even 6400 Hz. In both cases there are built-in filter with 1420 or 2840 Hz cutt-off frequency. As this accelerometer have internal mu...

Dfsd .1 by Associate
  • 1167 Views
  • 1 replies
  • 0 kudos

LIS3DE substitute

Hi, what is the natural replacement for the obsolete LIS3DE?Is there a model pin to pin compatible and software compatible?Thanks.

pb.11 by Associate
  • 1098 Views
  • 1 replies
  • 1 kudos

Resolved! L3GD20H fake IC issue

It is flight controller board for drone.In the schematic is written it is L3GD20H. Is it correct?I think it is fake chip.Also output data was not good in changing temperature environment.

0693W000008wLq1QAE.png
yundy by Associate
  • 1502 Views
  • 1 replies
  • 0 kudos