cancel
Showing results for 
Search instead for 
Did you mean: 

I have 2 versions of accelerometers for testing: First: Labelled LIS2DW12 works well, no problems Second: not labelled, same physically, but no joy. First has QR code with letter "T" on top. Second has QR with "M" on top. Can someone identify second?

DO'Sh.2
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Hi @DO'Sh.2​ ,

It should be the IIS2MDC part number. If so, the two devices are quite different, so you have to use different drivers to communicate with them. You can check the respective datasheets and the Github drivers for the correct interface of this other product.

But to be sure of the right part number, in case you are testing the parts soldered on ST adapters, please note that for the LIS2DW12 it is called STEVAL-MKI179V1, while the one for the IIS2MDC is named STEVAL-MKI185V1.

-Eleon

View solution in original post

2 REPLIES 2
Eleon BORLINI
ST Employee

Hi @DO'Sh.2​ ,

It should be the IIS2MDC part number. If so, the two devices are quite different, so you have to use different drivers to communicate with them. You can check the respective datasheets and the Github drivers for the correct interface of this other product.

But to be sure of the right part number, in case you are testing the parts soldered on ST adapters, please note that for the LIS2DW12 it is called STEVAL-MKI179V1, while the one for the IIS2MDC is named STEVAL-MKI185V1.

-Eleon

Thank you Eleon,

I checked your suggestion and you are correct.

Thank you very much for your prompt response.

All the best,

Donal

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.