cancel
Showing results for 
Search instead for 
Did you mean: 

lis3dsh Wakeup

MKS
Associate II

hi stm,

i have studied lis3dsh app note,

i didn't understand complete configuration for wakeup state machine , like after setting the registers to the specific value , interrupt will be generated , how to make it periodic interrupt , what are all the things need to be done to get an interrupt from wakeup can anyone please explain briefly , like what i need to do if i want to configure wakeup state machine.

Regards,

Manjunath

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
JHeik.1
Associate II

Did you ever get it sorted out? I'm having the same issue, my state machine only triggers INT1 once and I have no idea why. The command 11h should return the state machine to the start but looks like it doesn't. I followed the APP note A3393 and the wake up example.