MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SensorTile.box - Programmer adapter board and cable

Hi!Just purchased a SensorTile.Box, and moving now to use it on Pro Mode.On the SensorTile.Box user manual, it is mentioned that the product includes an adapter board - however, the one that I purchased did not include one. Does anyone know how can I...

MCach.1 by Associate II
  • 2913 Views
  • 6 replies
  • 0 kudos

VL6180 and 3143 Infrared Transmitting Acrylic

Sensor: VL6180Material: 3143 Infrared Transmitting Acrylic 3mm thick. Using API?: No. My own code using the data registers.Problem: Need an object in path only if using coverI currently have the VL6180 setup and working well in open air from a previo...

TMang.1 by Associate
  • 1959 Views
  • 3 replies
  • 0 kudos

UNICLEO GUI BLE connection problems

hello, I have programmed my sensorTile with ALLMEMS1 and would like to connect it with UNICLEOGUI via Bluetooth. I have connected the sensor to the PC via Bluetooth and it is connected correctly, but unfortunately, UNICLEO does not recognise my senso...

CRoma.11 by Associate II
  • 1905 Views
  • 4 replies
  • 0 kudos

Resolved! ISM330DHCX SDO_Aux wiring

Hello,I have a question about the configuration of the SDO_Aux pin. The datasheet of the ISM330DHCX suggests to leave the pin unconnected or connected to VDD_IO . Which is the most stable configuration?Thanks !

NBesn.1 by Associate
  • 928 Views
  • 1 replies
  • 0 kudos

Resolved! SensorTile Box- MKSBOX1V1

Hi, Am trying to connect SensorTile Box Using St-Link to flash the Program. But When I connect in DFU mode "USB" is getting detected, but through ST-Link V2, the serial numbers getting detected but am not able to connect. It says "STM32 Target not...

0693W000008zlgwQAA.jpg 0693W000008zlgNQAQ.jpg

Resolved! setting up test for wake up options on LIS2DW12

Hello, I want to set up checks for HP filter mode, relative reference mode and absolute reference mode in the device LIS2DW12(according to the document ST released.However I do not understand how should I see the difference between the modes.Can you ...

Msaga.1 by Associate II
  • 4142 Views
  • 9 replies
  • 0 kudos

LIS2DW12 high current consumption

Hi,We have STMicroelectonics LIS2DW12 accelerometer on our custom board which has nRF9160 SiP from Nordic Semiconductor and we are using the nRF Connect SDK which runs on Zephyr OS. Here are the LIS2DW12 driver codes of the nRF Connect SDK / Zephyr: ...

0693W00000AMew4QAD.png
APaan.1 by Associate II
  • 6336 Views
  • 12 replies
  • 3 kudos