MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Software library for interpreting PCM Data from MEMS Microphone

Do you have a software library or information how to interpret the converted PCM audio data? My project goal is to detect the accoustic level inside offices. Therefore I use the mems microphone mp34dt05-a and convert the incoming PDM Data to PCM data...

SWink.1 by Associate
  • 1579 Views
  • 2 replies
  • 0 kudos

Resolved! Cleaning a board with MP34DT05TR-A

Hi, we started using MP34DT05TR-A on our board, and as part of the manufacturing of the board we used to clean the board from flux residues after the assembly process, to prevent corrosion and leakage.I know that the MEMS microphones may be problemat...

AZ.2 by Associate II
  • 1935 Views
  • 2 replies
  • 0 kudos

Do you sell pressure sensors that measure up to about 2260 hPA?

I checked this page because I have size constraints but they max out at 1260 hPA. I need something that measures up to about 2260 hPA. Do you have something like this that I'm just not finding, or know of someone that does? Thanks for the help!

SWhit.5 by Associate
  • 1473 Views
  • 2 replies
  • 0 kudos

L3GD20HTR compatible pin-to-pin

Good morning,I am writing because I need to find an alternative to the L3GD20HTR component.Is there a compatible pin-to-pin alternative?Regards

GInte.1 by Associate II
  • 1828 Views
  • 3 replies
  • 0 kudos

lis3dh and lps22hb sensors trouble

Hello everyone!Got lis3dh and lps22hb on the custom board with F411 MCU. Use FIFO modes with both sensors. After getting interrupt on INT1 (lis3dh) and DRDY (lps22hb) pins MCU executes samples reading using DMA. Also got mutex for handling SPI bus ac...

0693W00000ANF79QAH.png 0693W00000ANFATQA5.png
AAlex.8 by Associate II
  • 3418 Views
  • 9 replies
  • 0 kudos

LIS2DW12 - orientation bit raised

Hello, I understand from the data sheet that once there is a certain acceleration value in one of the axis that is greater then the threshold and the value at the other axis is lower then the threshold, the orientation bit of the first axis (with val...

Msaga.1 by Associate II
  • 2455 Views
  • 9 replies
  • 0 kudos

Resolved! STTS22H I2C addressing

Hello,I have started working on the STTS22H and noticed that, at least for my part, the datasheet I2C addressing directive seems to be inverted. Aside from the fact that the datasheet and the evaluation kit have different addressing directives, the e...

nilotnas by Associate II
  • 2445 Views
  • 5 replies
  • 0 kudos