MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why does LPS25HB show wrong pressure value?

I'm using LPS25HB in my card. I can take correct temperature value but I can't draw pressure data as correctly. It show me that my Pressure is approximately 500 hpa but actually my pressure value is approximately 500 hpa. Is there any solution for th...

OCICE.1 by Associate
  • 1262 Views
  • 1 replies
  • 0 kudos

Resolved! How to use IIO triggered buffer?

I use ASM330LHH as Linux IIO.Source and DTS were added.We found that /sys/bus/iio also added a device.I also checked reading data in direct mode from sysfs.Therefore, I think there is no problem with the H/W connection.​I want to use Trigger mode to ...

0693W00000ANUmLQAX.png
Simon.Ko by Associate II
  • 5004 Views
  • 4 replies
  • 0 kudos

Resolved! Why do I get "There was an error loading the App on the board." when I attempt to load any of the example apps?

I am using the SensorTile.box that I just received today. I am using the ST BLE Sensor app Version 4.10.0 on my Pixel 4a downloaded from the Google Play Store. I get the same error on my Pixel 1. The blue LED flashes when the attempt to load is being...

PWood.1 by Associate II
  • 1666 Views
  • 1 replies
  • 0 kudos

VL53L0X Divide by Zero error in API

Hi all, Got a divide-by-zero exception whilst porting the API to the ESP32. The error occurs at line ~1960 in vl53l0x_api_core.c in this bit of maths: sigmaEstRef = VL53L0X_isqrt((cDfltFinalRangeIntegrationTimeMilliSecs + ...

RMill.3 by Associate
  • 2190 Views
  • 3 replies
  • 1 kudos

Resolved! LIS2DH Raw output to Temperature conversion

I saw below topics.How can i see discussion 71915817?***The datasheet doesn't specify how to convert register (OUT_TEMP_L (0Ch), OUT_TEMP_H (0Dh) ) data to actual temperature. let's say for example if reg 0x0c = 0x7 value and reg 0x0d = 0x00 value, t...

BBQ by Associate II
  • 1482 Views
  • 1 replies
  • 0 kudos

How can I diferentiate and detect continous motion of an object from vibrations/instant shocks on an object from by using LIS2DH12 sensor?

I'm trying to detect which product is being carried by crane by using LIS2DH12 for motion detection of steel coil products.  Because of the environmental vibrations or instant shocks created while handling the material in the stockyard I cannot diffe...

OTura.1 by Associate
  • 1606 Views
  • 3 replies
  • 0 kudos

Resolved! If Hang up I2C interface of the LIS2DH

If Hang up I2C interface of the LIS2DH, How can i reset the device except VDD OFF/ON operation?I am considering to send 9-clocks to the SCL of the LIS2DH.

BBQ by Associate II
  • 1568 Views
  • 1 replies
  • 0 kudos

Sinc Filter Order and value output of DFSDM

Hello dear ST-Forum,I'm currently working on DFSDM and MEMS-Microphone and am trying out the sinc filters. By changing the filter order e.g. from filter order 1 to filter order 3, the values increase dramatically. I have not found any proper calculat...

crackl1ng by Associate III
  • 1658 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.