User Activity

Certain things which are unclear are :1) When I increase the size of the PDM buffer and PCM buffer say to 2000 ,4096 to collect more samples for storing to convert them into a larger file into.wav or mp3 , I find no creation of the file in SD card .T...
The Acquired PDM signal is from VM3000 mic and PDM2PCM conversion using stm32f745?could the acquired values be played as loopback to verify whether the acquired sound is in audible frequency to human ears? How could this be validated? all suggestions...
There is something missing upon receiving junk .How do we keep the count of how much response will be received in advance ? should any flags be set to check whether the response received is correct and clear upon not receiving proper response , bit ...
The help will be greatly appreciated . I have to write this raw data extraction of PCM values in onto sdmmc sd card . And could anyone explain me how does the PDM2PCM functions for the mems than ST PDM microphones? I usually find examples of stm32 co...