2021-02-17 2:12 PM
Hello,
I am trying to understand how the PDM_Filter() function works.
If I am using 48Khz with a decimation factor of 64 and a output samples = 16
If I call the function like this...
uint16_t MidBuffer[16];
uint16_t pdmRxBuf[128];PDM_Filter(&pdmRxBuf[0],&MidBuffer[0], &PDM1_filter_handler);is the MidBuffer a 16 bit array or a 16 byte array
I am trying to store the PCM data into bytes that I can eventually send out of my UART.
Could anyone please help explain this to me? I have read the app notes and am still confused.
my configuration is below
void MX_PDM2PCM_Init(void)
{
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/**
*/
PDM1_filter_handler.bit_order = PDM_FILTER_BIT_ORDER_MSB;
PDM1_filter_handler.endianness = PDM_FILTER_ENDIANNESS_BE;
PDM1_filter_handler.high_pass_tap = 2104533974;
PDM1_filter_handler.in_ptr_channels = 1;
PDM1_filter_handler.out_ptr_channels = 1;
PDM_Filter_Init(&PDM1_filter_handler);
PDM1_filter_config.decimation_factor = PDM_FILTER_DEC_FACTOR_64;
PDM1_filter_config.output_samples_number = 16;
PDM1_filter_config.mic_gain = 0;
PDM_Filter_setConfig(&PDM1_filter_handler, &PDM1_filter_config);
/* USER CODE BEGIN 3 */
/* USER CODE END 3 */
}
2021-02-18 12:33 AM
Hi @kcire L. ,
for the PDM_Filter() function description, you can find references in:
But is this post related to this other one?
If so, can you check if that answer can be at least partially valid also for this post?
-Eleon