MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Calibration using MotionAcc library

I am using the industrial IIS2DH accelerometer in our vibration analysis product. I am collected data using the data-ready interrupt. For improving data accuracy I want to perform some calibration on data. I have found the following document. "Gettin...

Resolved! LIS3MDL Power Down Mode Issue

Hi,We are using LIS3MDL in our application and current consumption in Power-Down mode is 0.2mA which is quite high but it should be 1uA as per the datasheet.Any suggestion on why I am unable to achieve 1uA level as mentioned in the data sheet?Regards...

SKund.1 by Associate II
  • 5557 Views
  • 13 replies
  • 0 kudos

LIS2DH Raw output data noisy

I am reading the 3-axis data while turning on Inverter and cold cathode tube.The 3-axis data is too noisy. Is LIS2DH affected by external noise?Also, How can i reduce the noise on the raw data? (e.g. Exrta sheelding)

BBQ by Associate II
  • 1199 Views
  • 1 replies
  • 0 kudos

Problem while programming with Algo builder

Hi,I use Algo Builder to test the sensortile.box, but I can't program the board using the algobuilder software (after I have compiled) in order to test the functionality, even if it seems to be possible to program the microprocessor using directly ...

0693W00000AODlwQAH.png 0693W00000AODmVQAX.png 0693W00000AODmkQAH.png 0693W00000AODmuQAH.png
CDent.1 by Associate II
  • 22406 Views
  • 19 replies
  • 0 kudos

LIS3MDL large power consumption

Posted on June 22, 2016 at 19:45I am using the LIS3MDL magnetometer on a custom PCB I recently designed.  In addition to the sensor, the PCB has an STM32F101 and a HopeRF LoRa radio.  I am measuring current consumption by the LIS3MDL much larger tha...