MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

AIS2DW12 normal functioning

Hi everyone,I have run into some problems reading any data from the AIS2DW12 and I would like to know if anyone has had the same issue. I can read the Device ID through I2C but I am not able to read acceleration or temperature data. So my question is...

SLEWI.11 by Associate
  • 1078 Views
  • 1 replies
  • 0 kudos

TESEO-LIV3F gps interface with QN9080 MCU

Hi,We are using LIV3F module.. We have mounted components as per the schematics (with Part#W3011 as attached). We have tested module on Roof top for 30 minutes (In Hyderabad India). After power on, we are receiving packets GPRMC, GPVTG, GNGSA (as att...

0693W00000BbV8dQAF.png 0693W00000BbV8nQAF.png 0693W00000BbV8xQAF.png 0693W00000BbV92QAF.jpg
Snagu.11 by Associate II
  • 1572 Views
  • 2 replies
  • 0 kudos

NUCLEO-IKS02A1 and Unicleo-GUI

Hi All,has someone already connected this demo board with the Unicleo-GUI?The code runs in debug, I can get data out on a console, but the GUI would never regognise/find my board... :anxious_face_with_sweat: .The IDE is STM32CubeIDE running on Win7, ...

FBitt.1 by Associate II
  • 3040 Views
  • 6 replies
  • 1 kudos

Resolved! LIS2DW12 orientation bit

Hello We are working with accelerometer LIS2DW12.according to the diagram in the data sheet. if the accelerometer is in this state, will we see the zl \ zh orientation bit raised? 

0693W00000BbSwVQAV.png
Msaga.1 by Associate II
  • 1137 Views
  • 2 replies
  • 0 kudos

MotionFX_initialize() hangs

I've added motionFX to my project, which is an STM32F446, and i2c attached LSM6DSOX. I can read/write to the IMU using traditional methods (I2c) but I wanted to utilize the motionFX library, and when I initialize, the debugger hangs at the initialize...

Resolved! Which INEMO has the best performance?

Hello everyone,I am looking for the best IMU to use for a robotics project and I cannot decide which iNEMO is better.If I compare ASM330LHH, ISM330DHCX, ISM330DLC, LSM6DSRX it's hard to tell which one will perform better.I am looking for the one that...

LIS3MDL always output magnetic data 0 wrongly

Hello, support team.​In my design, I use 4-wire spi to transfer data between STM32F407 and LIS3MDL.Here is my configuration to LIS3MDL.CTRL_REG2 0x40 //Full-scale selection ±12 GaussCTRL_REG1 0x02 //XY low-power mode ODR 1000HzCTRL_REG4 0x00 //Z l...

PFeng.1 by Associate
  • 1187 Views
  • 1 replies
  • 0 kudos

LSM6DSOQTR datasheet

where could i find the LSM6DSOQTR datasheet?Is there any different between LSM6DSOTR and LSM6DSOQTR? thanks.

LKUO.1 by Associate
  • 1435 Views
  • 1 replies
  • 0 kudos

Resolved! LIS2DW12 axis orientation (sign)

Hi,I have a very simple (read: stupid) question in regards to the LIS2DW12 asix alignment (sign).I have implemented my own driver, but it is heavily based on this code: https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/lis2d...

0693W00000BbGhiQAF.png 0693W00000BbGjFQAV.png
CThue.1 by Associate II
  • 2733 Views
  • 4 replies
  • 0 kudos