MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! IIS2DH Z-axis not changing - stuck in mid value

I trying to find a solution as to why the Z-axis on the accelerometer is not responding. It is "stuck" at 0x80 for both high and low value. X- and Y-axis both work as they should. I can disable the Z-axis and it goes to 0x0. I set block update, the 3...

PJaco.11 by Associate
  • 1723 Views
  • 3 replies
  • 0 kudos

Velocity calculation in IIS3DWB vibration sensor

I am trying to compute velocity from the acceleration values by configuring the my IIS3DWB vibration sensor at +-4g. The formula I am using to calculate the instantaneous velocity is V(t) = V0 + ʃa*dt.What I am experiencing right now is a drift in my...

NukulK by Associate II
  • 2058 Views
  • 5 replies
  • 1 kudos

Resolved! LSM6DSR ODR not accuracy

Hi.i am using LMS6DSR ,and use ODR is 208Hz,but,i found that i can't get 208 samples at 1 secend.and,i had confirmed that it only about 203 Hz from Interrupt signal.so,i want to know is that normal? i can't find information about error of ODR in d...

Pqing.1 by Associate
  • 1492 Views
  • 3 replies
  • 0 kudos

MPU6050 gyroscope not working correctly

I am using the bluepill board and was trying to compute the angle from gyroscope raw data. However, when I tilt the sensor, the angle measured doesn't change as expected. It's changing between 1.xx and 2.xx regardless of the tilt angle. The sensor is...

M7890.1 by Associate III
  • 11038 Views
  • 11 replies
  • 0 kudos

Resolved! Different perofmance mode of LSM6DSO32

Hi all,I'am working with an LSM6DSO32, I read this AN5473 at page 13 and 14 we have 2 tables comparing different operating modes. I have a question for gyroscope for example if I chosse ODR 208Hz with G_HM_MODE = 1 I'am in a normal mode, and if I set...

SBaro.11 by Associate III
  • 1899 Views
  • 3 replies
  • 0 kudos