MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cannot get the Data Ready Interrupt working on the LIS2DE12TR.

We really need help getting the LIS2DE12TR to toggle the INT1 pin when new data is ready to be read. I've included the workspace bundle of our source. We are using a Cypress microprocessor.We can read the Whoami and successfully get 0x33.We've writte...

PDavi.5 by Associate
  • 961 Views
  • 1 replies
  • 0 kudos

Resolved! L3GD20H wrong gyroscope readings

I'm using L3GD20H on a flight controller board for drones.While conducting a temperature test that starts from -11°C and ends at 50°C, I observed a sharp rise/drop in gyro values at around 23°C. (The board stayed still the whole time inside a vibrati...

0693W000008wTuaQAE.png 0693W000008wTuVQAU.jpg
Gabsu by Associate II
  • 3139 Views
  • 9 replies
  • 0 kudos

MPU6050 gyroscope x and y axis data not right

I have collected 200 samples of the gyroscope raw data and get the average to calculate the offset. After that, I leave the sensor on table and try to read the raw data. The raw data read should be close to the average value that I obtained at the be...

0693W00000Bc2MEQAZ.png
M7890.1 by Associate III
  • 2759 Views
  • 4 replies
  • 0 kudos

Hello, I'm trying to import in my workspace a demonstration project provided by ST in X-CUBE-MEMSMIC1 and I get the error message below. How can I fix it? Thank you

Problem running CDT Scanner Discovery provider com.st.stm32cube.ide.mcu.toolchain.armnone.setup.CrossBuiltinSpecsDetectorError serializing language settingsInternal error while trying to serialize language settingsCannot create file, access denied: C...

MSant.11 by Associate III
  • 1354 Views
  • 3 replies
  • 0 kudos

Connectivity problems between SensorTile.box and Matlab

I'm trying to establish the connection between the SensorTile.box and Matlab. When I search for the Sensortile.box with the proper Matlab command, I can see the device but then, when I try connecting it, I get an error. I tried the same with a Sensor...

MFilo.1 by Associate
  • 868 Views
  • 1 replies
  • 0 kudos

Resolved! How to reset sensortile Box ?

I flashed my sensortile box but it stopped working after that. ( no lights blinking ).I did a reset on it using STM PRG. But still even when i plug it in still no lights are blinking. Battery is connected but there is no light.

AMuee.1 by Associate
  • 1187 Views
  • 1 replies
  • 0 kudos