MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to distinguish LSM6DSO32X from LSM6DSOX by software?

Hi,how to differentiate both chips, if they have the same value for WHO_AM_I register?I know that I could read couple times the accelerometer values, calculate magnitude over all axis and check if the value is near 1g or 0.5g (assuming no movement du...

MMade.1 by Associate II
  • 1265 Views
  • 1 replies
  • 0 kudos

Burning up of STEVAL-STLCS01V1.

Hello Folks,Greetings. I have been using STEVAL-STLCS01V1 on one of my IoT project and for some reason have burnt a few of them. I am pretty sure there is no short between the pins as well as no design issue. Has some one faced something similar? It ...

SJosh.8 by Associate
  • 1438 Views
  • 3 replies
  • 0 kudos

Why current of LIS2DTW12TR is too high?

Hi,We are trying to measure total current of LIS2DTW12TR. We have circuit board which according to schematic in details. We have 60uA when we measure the current flowing on CN34.  But in the application notes of LIS2DW12 ( i know it is a different mo...

0693W00000FCHaeQAH.png

AN5201: ODR

Output Data Rate(ODR) It can be considered as the frequency of data update, and the data will not be updated between update intervals.

user1 by Associate
  • 1097 Views
  • 1 replies
  • 0 kudos

Resolved! problem with lsm6dsl free fall detection

Hi sir , I working with( LSM6DSL)STEVAL-MKI178V1 Dk board communicating with nrf52840 controller board.i am able work pedometer and significant motion and tilt detection these modes are working but i am trying to generate free fall detection but i am...

MRedd.3 by Associate II
  • 2170 Views
  • 3 replies
  • 0 kudos

I want to use two wake up inrterrupts at the same time. Thresholds and duration will be different. I cannot use it at the same time because I changed the register value while doing the settings.

I want to use wake up interrupt for two different thresholds at the same time,for example I want to give wake up threshold 1g for interrupt 1, I want to give 500 mg for interrupt 2. And duration will be different.I change the value of WAKE_UP_THS, W...

Iakgu.1 by Associate III
  • 1023 Views
  • 1 replies
  • 0 kudos

Resolved! X-NUCLEO-CCA02M2 interface with nucleo-f401RE

Hi, I am using X-NUCLEO-CCA02M2 microphone board with nucleo-f401RE for USB audio streaming. Can anyone share the details about interfacing pin connection(which I2S pin is used)?. My understanding is like timer is used to connect pdm clock with I2S...

KK Y.1 by Associate II
  • 1802 Views
  • 1 replies
  • 0 kudos